Part Number: ADS4222 Other Parts Discussed in Thread: ADC3643 Tool/software: hi sir
I need a ADC ,Spec as below
12Bits / Sample rate 50M/Paralle/+/-10V
did you have any advise?
thanks
Part Number: ADC3543 Other Parts Discussed in Thread: ADC3643 Tool/software: I'm developing a custom adc3543 board, which is required to have 18bit complex decimation-4 interface at 61.44 Msps.
3 questions I have.
1. In adc35xx EVM GUI, I can't set…
Other Parts Discussed in Thread: ADC3643 Hello,
My customer is looking for an ADC product for the following application.
* PD sensor(current) --> IV converter and OPAMP (0V ~ 2V)--> ADC (14bits or more)
Can you please recommend the best ADC product…
Part Number: ADC3644 Other Parts Discussed in Thread: ADC3643 , I'm wondering if the ADC3644 (and the ADC3643 if it different) is monotonic. The datasheets do not mention monotonic explicitly, but it puts the DNL at 0.5 typical and max of 0.97, which…
Part Number: LP-AM243 Other Parts Discussed in Thread: ADC3643
Iam trying to interface adc3643 with am243
1)so i configured registers of adc3643 using spi
2)is it possible to transfer data by mapping dataout pins and data_clock(130MHz) of adc to…
Part Number: ADC12DL040 Other Parts Discussed in Thread: ADC12D040 , , ADS4222 , ADC3643 Tool/software: Hi team,
Does TI have similar specs like AD9231? ADC12DL040 or ADC12D040?
But INL and DNL are worse than ADC12D040. Do you have a better solution…
Part Number: ADC3643EVM Other Parts Discussed in Thread: ADC3643 Hi,
I'm using the ADC3643EVM REV E with a ZC702 EVM board and in this context I'd like to use the FPGA_CLK instead of the ADC's internal clock. Following my last post ( e2e.ti.com/...…
Part Number: ADC3422 Other Parts Discussed in Thread: ADC3643 ADC3422: how to calculate input voltage vs digital output count - Data converters forum - Data converters - TI E2E support forums
Is there any document to guide setting for the analog input…
Part Number: ADC3643EVM Other Parts Discussed in Thread: ADC3643 , , CDCE6214 , ADC3662EVM Hi,
ADC35XX EVM GUI just allows to set 10 / 25 / 65 MHz as sample frequency for ADC3643 in ADC3643EVM.
I want to use a differente sample frequency. Is there…