Part Number: ADC3660 Hi TI,
I want to have linux driver for ADC 3660 to read the values from ADC into DMA and then from DMA to our application. pls share the link where we can find the Linux drivers for same. If not then please share Linux example…
Part Number: ADC3660 So I am able to read and write registers and configured the ADC3660 to output my real 16bit data in SDR one-wire mode.
Everything looked like it was working fine. I could turn on the ramp and capture it. adjust the ramp and see…
Part Number: ADC3660 Help needed
We have made a board 8 x ADC3600 with a FMC connection, connected to a Xilinx AC701
The first ADC3660 has the FCLK, the other 7 are data only
When I grab data from the first ADC3660 - it looks good
The…
Part Number: ADC3660 So here we go, manual operation of the ADC3660.
So the tristate buffer enable is on a gpio pin.
I wiggle the bits as prescribed in the data sheet and nothing.
Can't tell if I have a successful write and I can see the read was…
Part Number: ADC3660
Why the configuration files generated by GUI software have multiple configuration procedures, write to the same register multiple times, and write the same data content?
Part Number: ADC3660
1. Use the environment
The ADC3660 is configured with 1Wire, 16bit, FS=65MHz, DCCLKIN=65MHz, 16 complex Decimation
2. problems
External to the ADC a sinusoidal signal, ADC acquisition result is basically unchanged, is a…
Part Number: ADC3660 Other Parts Discussed in Thread: THS4541 On the datasheet it reads that the device operations from .5 Msps.
If we need to sample DC (or low frequency), will we still see the signal or will it be filtered out? (We still need to…
Part Number: ADC3660
In my custom board I am using this IC ADC3660 to read the voltage input , calculate the transient values and record in NAND flash. The ADC is controlled using SPI lines. I my case there was requirement of four ADC channel, so I…
Part Number: ADC3660 Hi Team,
I have 2 questions as follows.
[Q1] The customer would like to use the following specifications. - Decimation: 32 - Output mode: Real - Output resolution: 20bit - Output interface: 2-Wire
Is the OUTPUT RATE in this…