One correction or clarification after checking with the PADC team. The ADC3643 does also support a one wire TDM mode in addition to the somewhat unique parallel DDR mode. For 32 decimated output the rate is probably low enough to handle on AM4372. We…
Part Number: AM5706 Other Parts Discussed in Thread: AM5728 , ADC3660 , MATHLIB I am porting a working AM5728 application to a AM5706. Some of my GPIO's had to be moved in the transition so I have to change some control module register definitions. I am…
Hello Randall,
For future products, we can provide source code with the proper release approvals. However, as you pointed out, this evaluation platform was developed over 10 years ago, and I do not believe we have the ability to meet this new standard…
Part Number: AM5749 Other Parts Discussed in Thread: ADS8422 , ADC3660 , Hi,
I'm currently developping the interface between the GPMC parrelle port and an ADC (ADS8422). To fit with ADC requirement, I need to set the RdAccessTime and PageBurstAccessTime…
Part Number: AM5706 Other Parts Discussed in Thread: AM5728 , SYSBIOS , ADC3660 , MATHLIB I have a project that runs on a AM5728 that I am trying to port over to a AM5706. With a AM7705 in CCS I can connect to the ARM core and DSP core so I think I have…
Part Number: CDCEL913 Other Parts Discussed in Thread: ADC3660 ,
I’m using a 12 MHz crystal oscillator and a CDCE(L)913 clock generator chip to drive the clock signals into an ADC3660. The CDCE(L)913 datasheet mentions an on-chip programmable load…
Part Number: ADC3660EVM Hi,
I am using a linux utility "spidev_test" to write into ADC register. For example if I want to write a value of 0x6c at offset of 0x70 , I use the following command:- $ spidev_test -D /dev/spidev1.0 -s 1000000 -H -O…
Part Number: THS4541 Other Parts Discussed in Thread: ADC3669 , , LMH5401 , TINA-TI Hi,
Below is my schematic
Vocm is open and not connected below are my observed outputs
Q1 : as per datasheet VCM will be mid supply but why my output is at 2V ?
i have…