Part Number: ADC3662ADC3662: Replace ADC3663 with ADC3662. What modifications are needed for the low-pass and anti-reverse sections in the original front-end circuit? - Data converters forum - Data converters - TI E2E support forums
Part Number: ADC3662 Hello,
We are currently developing a system with ADC3662. We have some problems with it, and we want direct Texas support, if possible, regarding our problem. Please contact me, and I will share all the details. Thank you
Part Number: ADC3662 Dear TI,
We are using a ADC3662 in our design with complex downconversion. One thing not clear from the datasheet is which component, I or Q, is obtained from the sine and which one from the cosine of the local oscillator.
Thanks…
Part Number: ADC3662 Dear TI Technical Support Team,
I am writing to request urgent assistance regarding a critical issue encountered with the ADC3662 in our 4-channel synchronous acquisition system.
1. System Setup:
Configuration: 2x ADC3662…
Part Number: ADC3662 Other Parts Discussed in Thread: ADC3663 , Replace ADC3663 with ADC3662. What modifications are needed for the low-pass and anti-reverse sections in the original front-end circuit? Below are two screenshots of the front-end schematic…
Part Number: ADC3662ADC3662schematic.pdf Hello expert,
The schematic of ADC3662 is attached. However, there is a bug on SPI happened. The CLK is normal however the data can not be received. Could you help to check the schematic for us?
Many thanks…
Part Number: ADC3662 Tool/software: Hi
I have a question about the ADC3662.
Is there any specification for terminal processing when chB is not used?
I couldn't read it from the data sheet.
Best Regards, Kato
Part Number: ADC3662 Tool/software: Hi,
I want to connect ADC3662 to FPGA but I am struggling to find how can I drive sampling clock inputs CLKP, CLKM.
What logic levels and/or driver I must use to have best performance? I read the datasheet but there…
Part Number: ADC3662 Tool/software: Hi,
is there always a hardware reset needed after power-up phase?
If yes, would it also be possible to keep the RESET pin at high from beginning, so:
Thanks for help!
Part Number: ADC3662 Other Parts Discussed in Thread: THS4541 In adc3662`s datasheet, chapter 6.6 say that input full scale is 3.2 Vpp and input commom model voltage is 0.95V. So the input range is from (0.95-1.6)V to (0.95+1.6)V. Is it right? However…