Part Number: ADC3663 Other Parts Discussed in Thread: TINA-TI Hi, Due to another issue I connected a high speed differential probe on the input of an ADC3663 (AIN_P vs. AIN_N). The signal looks like the close by filter capacitor (120pF) would be discharged…
Part Number: ADC3663 Hi Team,
we need to perform SI analysis for ADC3663IRSBR mentioned part number so please provide IBIS model for simulation
Thnaks & regrads
Diwakar
9686119935
Part Number: ADC3663 Hello, We are using ADC3663 for the settings : Sampling Clk = 20MHz, 2-wire, 16-bit, Bypass mode , wherein the DCLKIN = 80MHz is given to the ADC. When measuring the Output clk, DCLK = 80MHz but aren't receiving any FCLK, also no…
Part Number: ADC3663 Other Parts Discussed in Thread: LAUNCHXL-F280049C , TMDSFSIADAPEVM Hello,
I'm interrested by the ADC of ADC36XX family, in particular because they have a very low latency and a LVDS output connection.
In my project I want to…
Part Number: ADC3663 Other Parts Discussed in Thread: TSWDC155EVM Hi TI Support,
We are designing our hardware to interface ADC3663.
In this I am taking ADC3663 and TSWDC155EVM as references.
TSWDC155EVM, the LVDS lines are from a bank with VCCO25…
Part Number: ADC3662 ADC3662schematic.pdf Hello expert,
The schematic of ADC3662 is attached. However, there is a bug on SPI happened. The CLK is normal however the data can not be received. Could you help to check the schematic for us?
Many thanks…
Part Number: ADC3663 Tool/software: Hi team,
1. If it can cause interference and noise when the clock and the analogue devices are in an PCB layout area? Looking forward to your comments, thanks.
2. What do the marked blue and marked red mean?
Part Number: ADC3663
Tool/software:
Hello,
I am using an ADC3663 that is configured as follows and I am currently seeing a severely quantized 16-bit digital output when a continuous triangle wave is applied at the input
1. 2-wire mode 2. 16-bit…
Part Number: ADC3663 Tool/software: Hello,
We have a customer that purchased the ADC3663 from Digikey, they are asking about:
How do I connect an ADC3663 to Zynq UltraScale+?
Both boards have an FMC connector, although there doesn’t appear to…