It is an improved version of ADC3683 from which we hope to get better linearity. Since TI is the manufacturer in both cases, it is upto us to suggest the best ADC driver. Our current driver circuits closely resemble the ones suggested for ADC3683
Part Number: THS4541 Other Parts Discussed in Thread: ADC3683 , , OPA657 , OPA365 , THS4551 , ADC3683EVM , LM7705 , LM27761
Hi,
I'm designing a four channel optical detection front-end with OPA657 and THS4541.(connected to following ADC3683)
Main Circuit…
Thanks LI,
The temperature range of the ADC is covered in the datasheet, so all the specification numbers would include over PVT or process, voltage and temp.
So, if you feel you need more ENOB, then you may need to look at another part, like 16 or 18bits…
Lukas,
Please find python script attached. adc36xx_CDC.zip
585MHz should be possible if the CDCE can be configured for it. The 1170MHz will not work due to the output drivers of the ADC3683 being limited to 1Gbps.
Regards, Chase
Part Number: ADC3683EVM Other Parts Discussed in Thread: ADC3683 Hello, I have to questions about the ADC3683EVM:
(1) According to the datasheet of ADC3683 , the a nalog input BW is 900 MHz. However, according to the user guide of ADC3683EVM , there is a LPF…
Part Number: ADC3683EVM Other Parts Discussed in Thread: ADC3683 , For our application we would like to use the ADC3683 in 0p5 wire mode. I tried to set the software for the EvalBrd accordingly using real decimation with a decimation factor of 4 according…
Part Number: SN74CBTLV3251 Hi team,
Customer wants to use SN74CBTLV3251 as the multiplexer for ADC3683 in their MR application. Their sample rate is 50Msps.
Since there are very few parameters given in the SN74CBTLV3251 datasheet, can you help check whether…
Part Number: ADC3643 Other Parts Discussed in Thread: ADC3641 , ADC3683 , TSW1400EVM Hello,
We plan to use ADC3641 in our new project. I download the EVM design files and found it use FPGA to get ADC results,
1, Why use FPGA?
2, Can we use MCU to get it…