Part Number: ADCS7476
According to the timing diagram, SPI operates in a mode where CPOL=1 and CPHA=1 (with SCLK idle at high and sampling on the second edge). However, the data I read according to this configuration is incorrect.
Based on the textual…
Part Number: ADCS7476 The datasheet for ADCS7476AIMF/NOPB has an "Absolute Maximum Ratings" table on the tob of page 4 showing that the Maximum "Soldering temperature, infrared (10 sec) " is 215°C, but the "packaging information" table on page 28 shows…
Part Number: ADCS7476
Tool/software:
Dear Texas Instruments,
we use ADCS7476 in a new product. I develop firmware module for this converter.
From Q&A "ADCS7476: Datasheet specs regarding t8 (SCLK FE to SDATA high impedance)"
Q: (Angela Peters…
Part Number: AMC1336 Other Parts Discussed in Thread: ADCS7476 , TCA9539 , Tool/software: MNF: AMC1336 , AMC1303 ADCS7476 , TCA9539
We need "error information" for the parts. How can I find it?
Part Number: ADCS7476 Other Parts Discussed in Thread: ADC121S101 Tool/software: Hi team,
My customer is evaluating ADCS7476, and there is a question as below:
How many leading zeros on SDATA, three or four? I noticed that the wordings show four…
Part Number: ADCS7476
Tool/software:
Hi,
The ADCS7476 which I have is giving data as expected. To test the SPI signal, I have connected a variable power supply which can vary from 0 to Vdd(3V). The digital data which I am getting is double the corresponding…
Part Number: ADCS7476 Could you please help me to calculate the correct ENOB for ADCS7476? I am expecting a result below 12, but not sure which parameter to include in the notorious formula:
ENOB=(SINAD-1.76)/6.02
Shall I consider the minimum value…
Part Number: ADCS7476 Hi, expert,
The datasheet of ADCS7476 says the minimum digital input VIH is 2.4V, is this value a fixed one? Or this value will increase as the VDD? What if I use a 5V VDD and 2.5V digital input logic? Will it cause problems? …
Part Number: ADCS7476 Dear Support,
Good day,
Please help to check and advise date code and lot code based on the top marking.
Attached photo for reference. Thanks
Part Number: ADC121S101 Other Parts Discussed in Thread: ADCS7476 Hello,
The electrical characteristics of ADC121S101 is almost the same with ADCS7476. The differences between them is the ON resistance R1 of the multiplexer and track or hold switch…