Part Number: ADS1000-Q1 Hello,
My customer has been working on ADS1000-Q1. They'd like to convert the data by single mode which needs to change the converstion register to SC=1b from the default of SC=0b.
They see the same conversion time as shown…
Part Number: ADS1000-Q1 Other Parts Discussed in Thread: ADS1013-Q1 Tool/software: Hello,
My customer is investigating ADS1000-Q1 and they're wondering the input impedance dependency over temperature. Is it possible to show the data for non NDA customers…
Part Number: ADS1000-Q1 Looking at DS REV B OCT2015, just want confirm if the absolute maximum rating on item "Voltage to GND, VIN+, VIN-" is VDD+0.3 instead of just "0.3"
Part Number: ADS1000 Other Parts Discussed in Thread: LM35 , LMT87 Hi,
We are using an ADC ADS1000 with a LM4132EMF-3.3/NOPB to generate power supply and reference to the ADS1000. We also have an analog multiplexer TMUX1208PW to select one from the…
Part Number: ADS1000 Hi,
My customer is using ADS1000A0IDBVT to send the digital value the uP when a certain device is connected or disconnected. When the temperature of the ADC rise to ~ 50 degree C, the ADC starts railing to full scale causing false…
Hi zong shu,
As for reading operation,
1. Need to confirm your I2C address is 1001000 or 1001001.
If the chip has package marked BD0, it is 1001000
If the chip has package marked BD1, it is 1001001
2. Only need to focus on 3 byte.
– First…
Part Number: ADS1000-Q1 Other Parts Discussed in Thread: ADS1000 Hi Team,
Is it ok to drive the ADS1000-Q1 with a high Z input 10kOhm range?
Thanks, Mitchell
Part Number: ADS1000 Hi All
I working in PIC Micro controller , write 0x93 address (slave) ADS1000 not acknowledging . Please give coding routine and circuit diagram interfacing ADS1000 . Different controller I tried.
Regards,
Murali
Part Number: ADS1000-Q1 ADS1000-Q1 is used for NTC resistance temperature detection. The current connection method is single power supply.
How can the output of ADS 1000-Q1 be converted into voltage value? Is there a conversion formula or detailed documentation…