Part Number: ADS1013 Tool/software: Hello,
we are trying to read in single shot mode the ADS1013IDGS with an esp32 wrom 32 with I2C.
We are able to read the component register, but we often have an esp_timeout_err and we don't understand why.
Anyone…
Part Number: ADS1013 Other Parts Discussed in Thread: ADS1015 , ADS1014 There are some question below
Assume our VDD is 5V ,The FS (Full-Scale Range) is 5V or else (2.048V)?
There is no change for FS and LSB between single-ended / Differential Mode? …
Part Number: ADS1013-Q1 Hi Team,
Q1: Please check ADS1013-Q1 have VOH value.
Digital Output High would be what the digital lines are pulled-up to with the pull-up resistor, which should be DVDD.
Q2: DVDD is Max or Min for VOH value?
Thank you so much…
Part Number: ADS1013-Q1 Other Parts Discussed in Thread: ADS1013 , Hi Teams,
Q1: ADC pin internal resistance in ADS1013 uses common-mode or Differential, What difference between common-mode and Differential?
Q2: Please check ADS1013-Q1 have VOH value…
Part Number: ADS1013 Other Parts Discussed in Thread: ADS1015 , Hello, we switched from ADS1015 to ADS1013. I am aware of the HW differences. I thought that the FW would stay the same. We are using the same code that worked with ADS1015, but are now having…
Part Number: TMS320F280025C Other Parts Discussed in Thread: ADS1013
I want to set up baudrate between F280025c and ADS1013 but when I look F280025c datasheet I saw I can config 10kbps to 400 kbps and When I look ads1013 datasheet I saw 128 SPS to 3.3…
Part Number: ADS1013 Other Parts Discussed in Thread: ADS1014 Hello expert,
May I know when will the ALERT/RDY assert if config register setting is continuous-conversion mode? Thanks!
Best regards,
Ann Lien
Part Number: ADS1013 Hi,
I am using the ads1013 and I am having trouble accessing the device through i2c. It almost appears that I have a non working part but wanted to make sure I have everything connected correctly and I am writing to the correct address…
Part Number: ADS1013 hi,
we are considering using ADS1013/14 in a BMS system.
We want to measure 1 (or more) differential signal(s).
to preserve some battery we will drive I2C at minimum possible.
how low can we go to grant 3.3kSPS rate?
thansk a lot …
Hello Angel-san,
Thankyou for your reply. You comments sound like ADS1000-Q1 will be NRND soon. Would you please tell me the reason why you recommend ADS1013-Q1 even though ADS1013-Q1 is more expensive than ADS1000-Q1 which isn't good for customers w…