Part Number: ADS1013-Q1 Hi HI-Team
In my recognition that FSR is fixed at ± 2.048 V regardless of the VDD voltage. If it it correct, the error of the VDD voltage does not affect the error of AD conversion. Is it correct ?
Best Regards, Koji Haya…
Part Number: ADS1013 Other Parts Discussed in Thread: ADS1015 , Hi team,
I replace ADS1015 in EVM with a ADS1013 because almost the same except some register and PGA setting. I replace U1 with ADS1013. But I have questions and issue below.
1. When I config…
Part Number: ADS1013 Other Parts Discussed in Thread: ADS1015 Hello,
i have one question regarding ADS1013.
Data sheet says, that rise and fall time of i2c signals must below <300ns.
In official i2c specification, there is written, that fast mode…
Part Number: ADS1013 Hi,
I am using ADS1013. A problem occurred with ADS1013. Please tell me how to resolve.
Data is acquired by I2C communication using MCU. The data is regularly converted in the single-shot mode, but it seems that the acquired value…
Other Parts Discussed in Thread: ADS1013 , ADS1015 Hi,
I am using ads1013 using in am335x. Is the same source i am using from ads1015 to ads1013. the same ads1015 i can use the same software logic.
is there any settings for this..
regards
Part Number: ADS1013 Other Parts Discussed in Thread: ADS1014 , ADS1015 Hi,
Could you tell me about tha information of ADS1013
How much is the value of reference voltage?
Best Regards,
Yuto Sakai
Part Number: ADS1013 Other Parts Discussed in Thread: ADS1015 , ADS1014 In single-ended inputs I read output and have: 1,4 [V] - 0x16A 1,2 [V] - 0x166 1,2 [V] - 0x141
...
I'm sure the input voltage, Ain1- GND, and my I2C is ok, what is wrong ?
Part Number: ADS1013 Hi team,
My customer wants to know the time from when 0 is written to mode bit until the first conversion ready pulse is output.
Please let me know.
Best regards, Fumio Nakano
Part Number: ADS1013 Other Parts Discussed in Thread: LM4040 , ADS1014 , ADS1114 I'm planning to use the ADS1013 in a new design. I will ground AIN1, and connect my single-ended signal to AIN0. My input signal range is 0.3V to 3.5V and it is very slow…