Other Parts Discussed in Thread: ADS1013 , PCA9306 Hi
I have a question about I2C interface of ADS1013.
ADS1013 has I2C interface and VDD supply is 2V to 5.5V.
Can this device communicate with 1.8V I2C interface if VDD of ADS1013 is 2V? Because the input…
Other Parts Discussed in Thread: ADS1013 , ADS1014 , ADS1015 Hi Team,
Please help for customer's questions.
1. What is the slave address if tieing the ADDR to GROUND? 0x90(write) and 0x91(read)? in datasheet table 5.
2. ADS1013 said thaat AIN0 and AIN1…
Hi Chase,
The schematic looks ok for the most part. To be able to measure single ended inputs however, the ADS1013 and ADS1014 require AIN1 to be connected to GND externally. You can read more about this in section 9.1.2 of the data sheet.
Best Regards…
Part Number: TMS320F280025C Other Parts Discussed in Thread: ADS1013 Hello, I am trying to make i2c communication using ADS1013 with epwm. The problem is that my SCL signal is always pull down after communication. The other problem I'm having is, I'm seeing…
Other Parts Discussed in Thread: ADS1013 , ADS1014 , ADS1015 Hi,
Can we configure ADS1013 ADC in single ended input mode. I have to connect two analog inputs w.r.t ground onto it. Datasheet says it serve no function to ADS1013/14. Have any one tried this…
Hi Scott
Thanks for the reply.
After confirmed with customer, customer said they don't need TLA2024EVM-PDK this time.
Instead, they want to know if there is program compatibility between TLA2021 and ADS1013.
Because customer used ADS1013 for prototype…
Part Number: ADS1118 Other Parts Discussed in Thread: ADS1014 , ADS1113 , ADS1013 , ADS1018 We're having a difficult time finding a suitable replacement for this ADC. Anyone have any ideas for sourcing this part, or a simple alternative? Nothing else seems…