Part Number: ADS1015 Tool/software: Hi,
I am currently evaluating the ADS1015 for a configuration using four single-ended input channels.
According to Table 7-1 in the datasheet, when the LSB size is set to 0.5mV, the FSR is listed as ±1.024V. In…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1120-Q1 Hi team,
The datasheet of ADS1015-Q1 and ADS1120-Q1 doesn't state DNL. May I know DNL of ADS1015-Q1 and ADS1120-Q1?
Best regards,
Shunsuke Yamamoto
Part Number: ADS1015-Q1 Tool/software: Hello, I would like to ask your company for some information about this chipADS1015-Q1, please see details below, thank you
Part Number: ADS1015 Tool/software: Hi Team,
We are using the ADS1015 ADC IC to detect sine and cosine analog signals from the sensor, which outputs a voltage range of 100mV to 600mV.
I have a question regarding the ADS1015: If the full-scale range…
Part Number: ADS1015 Tool/software: Please help provide the required data for the following table and attach the scanned documents of the IATF16949 certification. Thank you.
Manufacturer Name
Manufacture Part#
Part#
Description
Standard…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 , ISO1541 Tool/software: I'm working with a design using an ADS1015BQDGSRQ1 at 5V with an ISO1541QDRQ1 to interface with a 3.3V bus with a TMS320F28386 as the I2C bus controller. The ADS1015…
Part Number: ADS1015 Other Parts Discussed in Thread: TLA2024
Tool/software:
Hi experts,
May I learn from you what are main differences between ADS1015 and TLA2024 except temp range? Customer would like to choose a solution for temp sensing with…
Part Number: ADS1015 Tool/software: Hi team
We are connecting pressure and leak sensor to ADS1015 in single ended configuration. In 9.2.2.6 of datasheet example
calculation were provided for differential input. How we should do calculation for single…
Part Number: ADS1015 Hello,
We are using the ADS1015 to convert data from a sensor
We are using this configuration on the ADC
#define DEFAULT_VAL 0xC703
We made the reading in this way, but always give us the same digital value
else…