Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 Hi,
in the datasheet the recommended operating conditions for tempreature are:
-40°C to 125°C
but I cannot find the maximum recommended jucntion temeprature for the component.
…
Part Number: ADS1015-Q1
D ear, support team. Our customers are using ADS1015AQDGSRQ1 (Is the A suffix a custom grade?) The A suffix is not listed in the data sheet.
We are considering replacing ADS1015AQDGSRQ1 with ADS1015BQDGSRQ1 due to delivery problems…
Part Number: ADS1015-Q1
Hi team
I would like to ask that do our ADC portfolios support function safety?
1. Do our devices themselves support function safety like ASIL-B?
2. Or do our devices support the customer system function safety to be ASIL-B?
…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 Hi,
I am having issues using libiio to read from ADS1015.
I can get access to the context and the device. I can even enable the desired channels but when I run the function to create the…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 Hi TI-team
My customer wants to get the sorure code for operation.
Do you have ?
They want to use it as a reference for software development.
Best Regards, Koji Hayashi
Part Number: ADS1015-Q1 Hi team,
Could you advise if there is a recovery command sequence when I2C communication error occur?
For example (Start*N + stop condition)?
Is there any apps note for I2C of this device?
regards,
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 , ADS7049-Q1 , ADS7142-Q1 Hello TI
We are using ADS1015-Q1 in our ZF TRW Automotive ADAS application products (Camera), now we are looking for the equivalent alternative but smaller size device…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 Hi team,
I am considering to use ADS1015-Q1's I2C communication with MCU over Serializer and Deserializer as below.
ADS1015-Q1 <--> Deserializer <- Cable(I2C signal embedded into s…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 Hello
We try to configure the ADC in the following way :
At init we enable alert/ready interrupt by setting Hi_thresh register MSB to 1 and Lo_thresh register MSB to 0.
We write the config…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015EVM-PDK I could not find un-encrypted spice model of ADS1015-Q1 to simulate using SIMetrix .
Could you please help with un-encrypted spice model for the same As early as possible.