Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 Hi,
I am having issues using libiio to read from ADS1015.
I can get access to the context and the device. I can even enable the desired channels but when I run the function to create…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 Hi TI-team
My customer wants to get the sorure code for operation.
Do you have ?
They want to use it as a reference for software development.
Best Regards, Koji Hayashi
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 Hi team,
I am considering to use ADS1015-Q1's I2C communication with MCU over Serializer and Deserializer as below.
ADS1015-Q1 <--> Deserializer <- Cable(I2C signal embedded into serial…
Part Number: ADS1015-Q1 Hi team,
Could you advise if there is a recovery command sequence when I2C communication error occur?
For example (Start*N + stop condition)?
Is there any apps note for I2C of this device?
regards,
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1018 Hi team,
I plans to use ADS1015-Q1 for voltage monitoring purpose in single end configuration.
The rail of monitoring is 3.3V rail with resister divider and supply voltage for ADS1015…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015EVM-PDK I could not find un-encrypted spice model of ADS1015-Q1 to simulate using SIMetrix .
Could you please help with un-encrypted spice model for the same As early as possible.
Hi Joseph,
Thanks for your kind reply.
My customer has some additional questions as following.
1. What's the reference voltage of ADS1015-Q1 when using VDD=3.3V?
2. What's the tolerance of the reference voltage if the VDD range is 3.2V ~ 3.4V…
Part Number: ADS1015-Q1 Hi,
My customer is considering to use the ADS1015-Q1.
Theyare afraid of trouble after designing.
Is there any careful point that is not described on the datasheet ?
Best Regards,
Kuramochi
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS7950 , ADS7142-Q1 Hi team,
A customer reviews ADS1015-Q1 for two single ended key inputs, but the ADC conversion time between these two inputs should be short, not to lose the input by the…