Part Number: ADS1110 ESD contact 6kV shot on the GND, ADS1110 error. The high level of SDA signal is below 1V(normal is 3.3V)
the yellow wave is SCL, and the green wave is SDA.
Part Number: ADS1110 Hi team,
My customer wants to use the ADS1110, but they need to know the ESD spec, do you have some esd data of the device?
Thanks.
Part Number: ADS1110 Other Parts Discussed in Thread: TMP100 Hello all,
What is the input capacitance for the ADS1110 I2C Pins?
or is there a formula to determine this?
Other Parts Discussed in Thread: ADS1110 Hi,
I am using ADS1110 16-bit A/D converter to convert differential and single inputs coming from different sources.
In differential input mode where the signals are generated across the thermal disk (thermal…
Other Parts Discussed in Thread: ADS1110 Hi,
I have a problem with ads1110, the I2C SCL seems to pull the voltage down all the time. That was after everything was working properly for a few days.
The ads1110 is powered up every 30 minutes and will…
Other Parts Discussed in Thread: ADS1110 , ADS1113 Hi,
I just wondering what will happen if one of the input pin of ADS1110, let say, pin In+, if floating ?
In other word, what does the converter see if one of its differential input is floating…
Other Parts Discussed in Thread: ADS1110 Hi,
I want to know about the internal clock oscillator(275kHz) of ADS1110.
What is the tolerance of the internal clock?
Best regards, Seishin
Other Parts Discussed in Thread: ADS1110 I am currently working with the ADS1110, and I am unable to read the configuration register. I'm a able to read the first two bytes that make up the output register, and I can change the input voltage to the ADS1110…
Other Parts Discussed in Thread: ADS1110 , ADS1118 Hi,Sir:
I Ihave a circuit using the ADS1100 with for detect voltage,
when power turn off
the Input cueernt is 100mA @Vin: 3V
the Input cueernt is 140mA @Vin:5V
the Input cueernt value is more…
Hi Bunnarong,
It would seem as though the input is floating. Make sure you have good ground connections between the op amp circuit and the ADS1110. Pin 2 and pin 6 of the ADS1110 must have the same ground potential (or common point) as the op amp circuit…