Part Number: ADS1114 Other Parts Discussed in Thread: ADS1115 Hello,
I use 2 ADS1114 in I2C with a supply voltage of +5V. Both works because values, on serial interface, change in function of analog inputs.
I use arduino with IDE interface to test…
Part Number: ADS1114 What is the value of the reference voltage for the ADS1114?
There is no mention of the value of the reference in the datasheet.
In operation I am seeing a maximum output of 2.5V.
Datasheet section 9.3.3, Full-Scale Range and LSB size…
Part Number: ADS1114 Other Parts Discussed in Thread: ADS1115 , , ADS1115EVM-PDK Hello,
I am designing a board with the ADS1114. It does not have a reference board, but the ADS1115 does. It was my intention to buy that board, mostly because it would give…
Part Number: ADS1114 Other Parts Discussed in Thread: ADS1115 ,
Dear Sir or Madam. Hello, I am making our EVB.
I should use ADC 2channels. because of measuring a Voltage of between Load's positive and negative.
I used ADS1115 that has 4-channels-single…
Part Number: ADS1114 Other Parts Discussed in Thread: ADS1115 Hi,
Doubt 1.May I get the testing code of ADS1114 (like Arduino or Raspberry Pi )…?
Doubt 2.The slave address of ADS1114 has (0x48 - ADDR connected GND ; 0x49 - ADDR connected to VCC…
Part Number: ADS1114 Hi Sir,
I have give below my code for ads1114 writing and reading data from it with HAL i2c library for STM32L4S9AII board. But I get values not consistently.
So, please refer it and help me.
Thank you.
// Function " init_ADS1114…
Part Number: ADS1114-Q1 Other Parts Discussed in Thread: ADS1114 Dear experts,
I have a following quesition about I2C port of ADS1114-Q1.
Is there any damage on the device or any problem when switching on and off VDD of ADS1114-Q1 while supplying voltage…
Part Number: ADS1114 Hello,
does the usage of the ADS111x 's PGA reduce the common mode range?
With some ADCs this is the case.
Thank you in advance.
Regards,
Alen
Part Number: ADS1114 Other Parts Discussed in Thread: ADS1113 , ADS1115 , Hi,
Comparing the diagram of ads1113 with ads1114 and ads1115
It indicates a significant different input structure - ads1113 has no PGA in the input. Never the less the datasheet…
Part Number: ADS1114 Hi Team,
A customer noticed that the full-scale input voltage range of ADS1114 is ±6.144V. However, Section 7.1 states that the minimum and maximum analog input voltage are GND-0.3V and VDD+0.3V respectively. Is there a typo error…