Part Number: ADS1118 Other Parts Discussed in Thread: ADS112C04 , ADS112C14 Hi TI Team,
My current design is having ADS1118 and now I need to modify the hardware for 1.8V logic. Instead of using level translator I am planning to replace ADS1118 with…
Part Number: ADS1118-Q1 Other Parts Discussed in Thread: ADS1118 Hi team,
My customer is using the ADS1118 to extract the 2nd harmonic of a 50 Hz fundamental signal. However, the input signal contains interference from the 0.5th harmonic, 3rd harmonic…
Part Number: ADS1118 Dear Specialists,
My customer is considering ADS1118 and has a question.
I would be grateful if you could advise.
---
Could you please let me know the relationship between conversion time and DRDY status(High to Low) regarding…
Part Number: ADS1118 Hello E2E Experts,
Good day.
I found that when using the thermocouple measurement circuit provided by the ADS1118 datasheet to measure a 2MOhms resistance , it takes about 5-10 seconds to read stable data, and after removing the…
Part Number: SN74LV4052A Other Parts Discussed in Thread: ADS1118 Hi tech support,
We are designing a multi-channel thermocouple data collector that is used in plastic manufacturing industrial machine. We plan to use 2*SN74LV4502A and 1* ADS1118 to…
Part Number: ADS1118 Other Parts Discussed in Thread: ADS1018 , TLA2024 Tool/software: Hi expert,
Do we have new generation of ADS1118IDGSR? Customer want to know if we have cheaper and same performance devices or same price and better performance devices…
Part Number: ADS1118 Tool/software: Hi there,
We want to read Analog voltage ( 0-5V) which comes from display interface.
Can we use voltage divider as 3.3V to AIN1 channel for the part : ADS1118IRUGR ?
Ref Image:
Please, Advise.
Part Number: ADS1118 Other Parts Discussed in Thread: ADS124S08 Hello,
Currently I need to interface ADS1118 to linux based system.
I need Linux driver for ADS1118 and also It will be good to have some reference example application code for it.
…
Part Number: ADS1118 Tool/software: Hi team,
Could you tell us below information about electric characterictic value.
1,Minimum Differential input impedance @FSR=±0.256V 2,Maximum Differential input impedance @FSR=±0.256V
3,typical and maximu value…
Part Number: ADS1118 Other Parts Discussed in Thread: ADS1220 Tool/software: Hello All,
I was wondering if it is possible to use a RTD instead of a thermocouple with this chip or are there other chips available able to do the same job as the ADS1118…