Other Parts Discussed in Thread: ADS1118EVM , ADS1118 , ALLIGATOR Hello I am currently using an ADS1118evm hooked up to a Beagleboard
I just need to make sure I can get voltage readings from the ADC to the beagleboard.
For thw interface I am using…
Other Parts Discussed in Thread: ADS1118EVM , ADS1118 Hello,
I'm having trouble setting the configuration register on the ADS1118EVM using SPI. I've tried various combinations of Continuous/Single-Shot and samples per second, but haven't had any luck…
Other Parts Discussed in Thread: ADS1118EVM , ADS1118 Hi, I'm a newbie, just started to use an ADS1118EVM with the supplied demonstration software. It's working great, monitoring mV input on Ain1. Right-clicking the graph produced and choosing "Copy data…
Other Parts Discussed in Thread: ADS1118EVM , ADS1118 , ADS8320 , ADS1100 , ADCPRO ADS1118EVM looks like a good evaluation module that can be hooked easily to our dev board through SPI interface. However, ADS1118 only supports 860SPS, while we need to…
Part Number: ADS1018EVM Other Parts Discussed in Thread: ADS1118EVM , ADS1118 , ADS1018
All:
I have set up ADS1018EVM - had to update drivers manually via Device Manager using PAMB_USB_Driver_Install...
When I run "software GUI" from Eval Board…
Electrobud,
For the thermocouple measurement to be accurate, the two leads of the thermocouple and the cold-junction measurement must all be at the same temperature. Generally, the PCB is designed so that all three are close together, so the temperature…
Dany,
Just to make sure that you have this the ADS1118EVM is built like a thermocouple measurement application and you can find the user's guide here:
There is also a short cookbook circuit here:
Additionally you can find an application…
Hi Shubbam,
This is a rather broad question. In short, you should be able to use the ADS1118 to measure the voltages listed.
At a high level, for the inputs, I would have 2.5V on V_AIN1 and the "measuring voltage" (i.e. +1V, +1.8V, +3.3V, +5V) on…
I would like to translate this question.
I'm using ADS1118EVM. Sometimes I will observe temperature jump from 27.2℃ to 0 as shown below. But the actual temperature should remain constant. Why?
And what does dynamic, static mean?
Shreenidhi,
The ADS1118 should work fine for a thermocouple measurement. There's a lot of information about using this device for a thermocouple measurement. The ADS1118EVM has a thermocouple connection to make temperature measurements. The customer…