Part Number: ADS1120 Hello,
I have encountered a problem with the ADS1120 ADC. When measuring voltage, we observe a current flowing into the pin. In the path of this current we have protection resistors of 3.3 kOhm, and the current is about 10 nA. For…
Part Number: ADS1120 Our application runs the ADS1120 in single-shot conversion mode.
The sequence we originally tried to use is:
Issue START/SYNC command
Power up sensor
Wait for sensor to settle
Write mux and PGA configuration for desired…
Part Number: ADS1120EVM Hello, I have probably a silly question. I've been getting what seems to be unpredictable data output codes. I wanted to check and make sure that I got the wiring correct. From left to right, EXC- has the black ground/neutral wire…
Part Number: ADS1120 Other Parts Discussed in Thread: ADS112S14 Hello,
We are encountering the following problem with the ADS1120IPWR model: we need to read both the EU (10-180) and US (240-33) ohm sensors. As shown in the circuit diagram below, we…
Part Number: ADS1120 Other Parts Discussed in Thread: ADS1235 , ADS112S14 , ADS122S14 Hello, I'm looking for an ADC that'll work with a strain gage load cell. The ADS1120 was recommended to me. I plan on testing that with the evaluation board.
I'm wondering…
Part Number: ADS1120 Hi team,
I have two questions about using the ADS1120 in single-ended mode.
Question 1
Operating Conditions:
Using the ADC in single-ended mode (AVSS connected to AINN, AIN1 set as AINp input)
Power supply voltage: 5V…
Part Number: ADS1120 Other Parts Discussed in Thread: ADS112S14 , ADS122S14 Hi,
I want to use ADS1120IPWR for 4 wire RTD and voltage measurement together i.e. measure RTD signals in 4 wire mode using AIN3, AIN1, AIN0, REFP0 and REFN0 and perform voltage…
Part Number: ADS1120 Tool/software: To read the temperature with the Ktype sensor, I first send the 0x04 command to the IC and read and calculate the temperature. Then, when I send the 0x06 command to read the internal temperature, the IC reads again…
Part Number: ADS1120 Hi,
I am using ADS1120IPWR part in one of my design. I have configured ADC to measure single - ended inputs (0-5V).
I am providing AVDD - 5V and AVSS- Analog ground. As i am using the device in single-ended mode, can i get a…
Part Number: ADS1120 Other Parts Discussed in Thread: LP-MSPM0G3507 , SYSCONFIG , MSPM0G3507 Tool/software: Hi,
Does anyone know of any example code + library for ADS1120 ? I have LP-MSPM0G3507 and I work in CCS Version: 12.8.
I found example code…