Part Number: ADS1120 Tool/software: To read the temperature with the Ktype sensor, I first send the 0x04 command to the IC and read and calculate the temperature. Then, when I send the 0x06 command to read the internal temperature, the IC reads again …
Part Number: ADS1120 Tool/software: Hello, I'm looking for a microcontroller that'll pair with the ADS1120. Also is TI able to put these together on a printed circuit board? Thank you.
Part Number: ADS1120
Tool/software:
Dear Technical Support Team,
My configuration is 3-wire RTD with ADS1120.
I have some questions.
Q1)
When it is shorted circuit or open circuit condition, is it possible to measure some kind of temperature? If so, what…
Part Number: ADS1120 Tool/software: Hi, team
I want to simulate using LTspice of ADS1120.
I found that you are responding that there is no ADS1120 spice mode before about a year.
Does it still not exist now?
If not, What do you have a similar spice…
Part Number: ADS1120 Other Parts Discussed in Thread: LP-MSPM0G3507 , SYSCONFIG , MSPM0G3507 Tool/software: Hi,
Does anyone know of any example code + library for ADS1120 ? I have LP-MSPM0G3507 and I work in CCS Version: 12.8.
I found example code for the…
Part Number: ADS1120 Tool/software: I am using the ADS1120 to measure RTD (Resistance Temperature Detector) values. I am utilizing AIN1 and AIN2 as the input channels and configuring IDAC1 and IDAC2 for excitation current at 1000 μA (1 mA). Additionally…
Part Number: ADS1120 Other Parts Discussed in Thread: MSPM0G3507 , , SYSCONFIG Tool/software: Hi,
could someone advise me how to override this function (for MSP430) ReceiveByte ADS1120 fot MSPM0G3507 with DL_SPI_transmitData8() and DL_SPI_receiveData8() ?…
Part Number: ADS1120 Hi,
I am using ADS1120IPWR part in one of my design. I have configured ADC to measure single - ended inputs (0-5V).
I am providing AVDD - 5V and AVSS- Analog ground. As i am using the device in single-ended mode, can i get a full 16…
Part Number: ADS1120-Q1 Tool/software: Hi team,
When the ADS1120-Q1 is powered on, the ADC sampling fails.
Fault description: Our software will send a reset command to the ADC chip via SPI when powered on, set the value of the 02h register to 0x10, and…