Part Number: ADS1120 Hi my customer want to konw if the case of using 2ch differencial input, the max sampling rate is still 2kSPS at Turbo mode?
Best Regards, NY
Hi Joachim Wueker,
Yes, we have made some changes as per the suggestions, and for further accuracy improvement, we are processing the calibration.
Thanks for the support!
Part Number: ADS1120 Other Parts Discussed in Thread: ADS131E04 , ADS114S06 Hi expert,
My customer is using the AFE that is Pseudo-Differential output as input signal,
In generally, Can they use the General Purpose differential input ADCs? or should they…
Part Number: ADS1120-Q1 Other Parts Discussed in Thread: ADS1120 , , ADS131B02-Q1 I want to use the differential input port of ads1120 as the input of both side of the shunt sampling resistor( range ±100mV), but I only have a positive power supply externally…
Part Number: ADS1120 Other Parts Discussed in Thread: ADS1220 , ADS114S06B , ADS124S06 , ADS1248 , ADS1148 Hi Team,
My customer is asking can ADS1120 output 0~FFFFh(16bit) for example, by setting registers when input is single end for positive signal only…
Hi, bob I want to close this thread with a thank you note. ADS1120S is working fine as of now. thanks for your overall support and quick replies. Your quality of support is indeed top-notch!
Part Number: ADS1120-Q1 HI Team,
8.3.11 System Monitor of the datasheet says:"Note that the system monitor function only provides a coarse result and is not meant to be a precision measurement"
Could you please provide the acuracy data of measuring…
Part Number: ADS1120
Hi Experts,
Good day.
The device ADS1120 has no reset pin; other than sending a RESET command, may we know what's the proper way to reset it? Does conducting power cycle to digital supply only would suffice?
Thank you.
Regards…
Part Number: Team,
I am still confused about the application of ADS1120, so I would like to list more questions:
1. What is the function AVDD and AVSS? Where do they connect to?
2. What is the function of VREF if choose internal VREF?
3. If AVDD is tied…
Part Number: ADS1120 Team,
Customer is using ADS1120 in the battery pack, and they need to use ADS1120 to measure bi-directional current. Now they are wondering whether ADS1120 could measure negative differential input signal? Customer have found that…