Part Number: ADS1120-Q1 Other Parts Discussed in Thread: ADS1120 I have a system with an ADC input of 3.3V. I want to protect my processor to max 36V. Do you have a circuit or integrated for this?
Part Number: ADS1120-Q1 Dear Team,
My customer is evaluating the ADS1120-Q1 with K-Type Thermocouple in their system. However, there is a slight difference in temperature between the actual thermocouple contact and the temperature sensor value inside the…
Part Number: ADS1120-Q1 Hi,
We measure with reference to AINn. I will therefore assume that we do an offset calibration with reference to AINn. Do we still need to do an offset calibration with reference to (AVDD + AVSS)/2? I do not really see the need…
Hi Furqan,
ADS112U04 and ADS122U04 are our only UART interface ADCs, and these are only available in Catalog Rating.
Our most comparable device with Automotive Rating would be ADS1120-Q1 data sheet, product information and support | TI.com .
This device…
Part Number: ADS1120-Q1 Other Parts Discussed in Thread: ADS1120 Hi,
I used the ADS1120 to measure thermistor (from 100ohm to 300kohm).
I used a ratiometric schematic, the voltage reference is AVDD = 5V. Component is configured to used the AVDD voltage as…
Part Number: ADS1120-Q1 Dear team,
My customer is evaluating the ADS1120-Q1 in their system. In the immunity test, they found that the internal temperature sensor value of the ADS1120-Q1 varied, around 1°C to 2°C variation, with exposures over 400MHz…
Part Number: ADS1120-Q1 Other Parts Discussed in Thread: ADS1120 Dear Team,
My customer is evaluating ADS1120-Q1 with K-Type Thermocouple with 38AWG (0.1mm diameter). The ADS1120-Q1 application is the same as "Figure 74. Thermocouple Measurement" of …
Part Number: ADS124S08 Other Parts Discussed in Thread: ADS1261-Q1 , ADS1120-Q1 Tool/software: Hi Expert,
My customer is looking for the solution with AEC-Q100 qualified in RTD measurement system. The RTD requirement we can refer to below screenshot from…
Part Number: ADS1120-Q1 Other Parts Discussed in Thread: ADS1120 Hi,
I have a question about the full-scale input voltage range for the ADS1120-Q1.
The inputs are configured as 4 channel single-ended input and the range would be from 0.3V to 4.7V. I just…
Hello Zsolt,
The ADS1114-Q1 would work for this, but you will need to provide a current source somehow. Here is a reference design that shows you how to do this for a space-grade device: https://www.ti.com/lit/ug/tiduf19/tiduf19.pdf . You could adapt this…