Part Number: ADS112C04 Hello, I'm working with the ADS112C04. I have a device that will at most output 80mV. Therefore, I can tune the PGA gain fairly high to improve resolution and reduce noise. The current output as measured by a volt meter is 50 mV…
Part Number: ADS112C04 Hello,
We are configuring the ADS112C04 to mesure its external reference voltage /4 (5V/4 = 1.25V) (MUX[3:0]=1100, gain bypassed=1)
Even though all the other self thests works, this one fails , giving us 0.5V . The Voltage between…
Part Number: ADS112C04 Dear, TI support Team. We are currently using AIN0-AVSS and AIN2-AVSS alternately in SINGLE-SHOT CONVERSION MODE. In order to use the CONTINUOUS CONVERSION MODE of ADS112C04, only 1ch, AINP, and AINN can be set for the channel designation…
Part Number: ADS112C04 Hi Team,
For the ADS112C04, are input offset voltage specs referred to the input of the part, or the input of the modulator? Just want to make sure I account for the selected gain factor correctly in calculations. For instance…
Part Number: ADS112C04 Hello
i am able to get the ACK if write a slave address and any other commands from the ADS112C04. every command which i wrote.
steps I am following :
1.reset the ADS112C04 by issuing the below command
<S>0x80 0x06 <P…
Part Number: MSP430FR5994 Other Parts Discussed in Thread: ADS112C04 Hello,
I am trying to read data from a ADS112C04. Therefore I have written functions that basically work like corresponding functions from eusci_b_i2c library but with repeated start…
Part Number: ADS112C04EVM Other Parts Discussed in Thread: ADS112C04 , ADS122C04
Hi, I'm jun hyeob in KOREA,
I wonder that i can use ads122c04 instead of ads112c04 chip on evm.
I mean, if i use jumper to connect the same pin map in evm and ads112c04…
Part Number: ADS112C04 dear
The voltage of PT1000 is read by means of 2-wire design,the voltage value of RTD is read. The external voltage is used as a reference. Do we still need to read the external voltage Vref?
thanks in advance
Part Number: ADS112C04 Other Parts Discussed in Thread: ADS1115 Dear Ti Engineers,
I`m planning to use the ADS112C04 for thermocouple (TC) measurement with an automatic power-on and off if the TC is connected or disconnected (See attached Schematic…
Part Number: ADS112C04 Hello..
I want to know how to read the data from the ADS112C04 ADC. First, I have given the slave address as 0X80, and after START/SYNC command as 0x08. what should I do after doing this I want to read the data continuously from…