Part Number: ADS114S06 SBAA201A ( www.ti.com/.../sbaa201a.pdf) doesn't mention the ADS114S06 (or similar) part numbers, so I am just wondering if this design guide also applies to this part.
Specificially section 3.4 and table 3-1.
Additionally, section…
Part Number: ADS114S06 We have 4 identical boards (same design, same configuration, same FPGA logic build). Simplifying the issue a lot - on 2 boards, the ADC starts up correctly and we're able to talk to it, and on the other 2, it does not.
We believe…
Part Number: ADS114S06 Other Parts Discussed in Thread: STRIKE , ADS124S08 Does the ADS114S06 (and family) use a switched-capacitor structure for the reference input? And is the reference input effectively "sampled" at the same time the analog input is…
Part Number: ADS114S06 Other Parts Discussed in Thread: ADS1147 Hi Experts,
I wrote a driver for this device in embedded c++. The ADC is used in continuous conversion mode, and the DRDY pin is polled to detect the end of each conversion, which starts…
Part Number: ADS1148 Other Parts Discussed in Thread: ADS114S06 , ADS1248 , , ADS124S06 The project I am working on requires us to determine if there is non-volitale memory (NVM) in any part we are using. At one point, we had picked another company's…
Part Number: ADS124S06 Other Parts Discussed in Thread: ADS114S06 , Tool/software: Hi,
Are ADS124S06 and ADS114S06 compatible for register map and DC / AC spcecs etc on datasheet?
I alredy use ADS124S06 (24bit) and develop software on MCU.
If I…
Part Number: ADS114S06 Other Parts Discussed in Thread: ADS124S08 Hello,
We have a battery powered system that we originally designed using the ADS124S08, we have recently switched to the reduced performance ADS114S06 and have noticed around 50 uA…
Part Number: ADS114S06 Tool/software: Hi, Staff
I have a question about the POR_Flag of the ADS114S06IPBS. When a power-on reset occurs, it becomes "1", but is it also set to "1" by a reset command or by a reset terminal?
regards cafain
Part Number: ADS114S06 Any idea where I could find the CMRR vs frequency graph of the ADS114S06 differential input? Also, the same for the PSRR of the internal 2.5V reference?
The datasheet only mentions values at DC or at 50/60 Hz.
I have an application…
Part Number: ADS114S06 Other Parts Discussed in Thread: DAC161S997 We've been testing a product that uses this ADC to convert a mV pressure transducer signal to 4-20mA output current with the DAC161S997 and a microcontroller.
When we apply a IEC 61000…