Part Number: ADS114S06 Other Parts Discussed in Thread: ADS124S08 Hello,
We have a battery powered system that we originally designed using the ADS124S08, we have recently switched to the reduced performance ADS114S06 and have noticed around 50 uA more…
Part Number: ADS114S06 Other Parts Discussed in Thread: DAC161S997 We've been testing a product that uses this ADC to convert a mV pressure transducer signal to 4-20mA output current with the DAC161S997 and a microcontroller.
When we apply a IEC 61000…
Part Number: ADS114S08 Other Parts Discussed in Thread: ADS114S06 , Dear Specialists,
My customer is considering ADS114S08 as substitute for ADS114S06.
These are pin compatible.
At the point of control signal, it is possible to use the same control signal…
Part Number: ADS114S06 Any idea where I could find the CMRR vs frequency graph of the ADS114S06 differential input? Also, the same for the PSRR of the internal 2.5V reference?
The datasheet only mentions values at DC or at 50/60 Hz.
I have an application…
Part Number: ADS114S06 Other Parts Discussed in Thread: ADS114S08 , ADS124S06 Hi Experts,
Our customer is developing a product using the 16bit ADC, ADS114S06. He is powering the ADC with a 3.3V unipolar supply. It is configured for single-ended input i…
Part Number: ADS114S06 Other Parts Discussed in Thread: ADS124S08
HI expert,
My customer would like to read the AD data between 0V and 3.3V 16bit( 8000h ( 0V )~ 7FFFh(3.3V) )with AVDD=3.3V and single end input.
They are considering the following configration…
Part Number: ADS114S06 Other Parts Discussed in Thread: ADS114S08EVM , ADS124S08 Please tell me about the output signal DOUT.
Product model number: ADS114S06 Evaluation board: ADS114S08EVM
We measured 3-wire RTD on the evaluation board and observed SCLK…
Part Number: ADS114S06 Other Parts Discussed in Thread: ADS124S08 , ADS124S06 , , ADS114S08 Hi team,
Could you provide the hex file for the follow example code
ADS1x4S08 Firmware Example Code : https://www.ti.com.cn/cn/lit/zip/sbac159
One of our customers said…
Hi Yash,
Thanks for the follow up and the resolution. Hopefully this will help someone else if they see something similar. The Electrical Characteristics Table on page 9 of the ADS114S06 datasheet shows the range of capacitive load stability for the internal…
Part Number: ADS114S06 Basic problem description:
For a given voltage input the ADC code generated is greater than expected.
Detailed problem Description:
10uA Burn-out current was selected on AIN3 and AIN4 pins via the System Control register. These…