Part Number: ADS114S08 Other Parts Discussed in Thread: ADS114S06 Hello ,
We followed the configuration of Multiple Two-Wire RTDs (Figure 15) in ours design. Also, as explained in the datasheet chapter 9, it is written: "As described in the Functional Block…
Hi Mukuno,
All three devices are capable of pseudo-differential measurements. The ADS131E04 is a rather large package (TQFP-64) but has simultaneous converters whereas the other two devices use a muxed input and a single ADC. Depending on the gain applied…
Part Number: ADS1248 Other Parts Discussed in Thread: ADS114S06 , ADS114S08 , ADS124S08 , ADS124S06 , ADS1261 , ADS1260 , ADS122U04 , ADS1120 , ADS1220 , ADS122C04 Hi,
I am looking for 24-Bit Analog-to-Digital Converters for Temperature Sensors similar to the…
Part Number: ADS114S06B Other Parts Discussed in Thread: ADS114S06 , ADS114S08B Dear Sir/Madam,
We have built a custom board using ADS114S06BIPBS to read PT1000 sensors. But we are having issues with SPI communication. The signal line from the MCU to ADS114S06…
Part Number: ADS114S06B Hi ,
1. i was working with ADS114S06B and it is interfaced to Raspberry pi using spi interface. i was to unable to read any data from ADS114S06B , i was in confusion that whether the device is working or not. can you please suggest…
Part Number: ADS114S06B Other Parts Discussed in Thread: ADS114S06 Hi expert,
1. Please help review schematic of ADS114S06B.
2. Could I directly use this schematic for ADS114S06?
6735.schematic.pdf
Regards and thanks.
Jiandong
Hi Kai, I am a part of Yash's team on this project. After this thread, we modified our design as such
However, very strangely, on applying 1kV L-E (balanced, all lines to earth), we find that the surge damaged the XTR and our microcontroller while…
Hi Cameron,
Yes, you can use the Full Scale Range (FSR) which is +/-5V when your reference voltage is 5V and Gain is 1.
Your signal is differential so you should not use the pseudo-differential configuration which is discussed in the section 3 of sbaa133a…
Part Number: ADS124S06 Other Parts Discussed in Thread: ADS1120 , ADS1220 , ADS114S06 Hi Sirs,
Please help on these questions.
Thanks.
1. While using single-end input, the int. PGA needs to disable or not? And if disabled the PGA, what the input impedance…
Part Number: ADS1120 Other Parts Discussed in Thread: ADS124S08 , ADS1220 , ADS114S06 I am looking for a sample code for the measurement of the temperature via 3 wire sensors like PT100/PT1000 or 2 wire sensors like NTC /PTC. I am a beginner with ADS1120…