Part Number: ADS114S06B Other Parts Discussed in Thread: ADS114S06 Tool/software: Hi team,
I would like to use the attached tool with ADS114S06B, but I cannot use it because some values are not in the datasheet. Is it possible to get this tool adjusted…
Part Number: ADS114S06B Hello guys,
One of my customers is evaluating ADS114S06B with 5V AVDD and 3.3V DVDD/IOVDD.
They want to shut AVDD only down to 0V for power saving. Is it no problem for the device If AIN0~5 and GPIO0~3 terminal voltage are shut…
Part Number: ADS114S06B Other Parts Discussed in Thread: ADS124S08 Hi Team
My customer is considering thermistor resistance measurement circuit using a constant current source (IDAC).
If customer touch the wiring connected to the thermistor during resistance…
Part Number: ADS114S06B Hi,
I have selected ADS114S06B 16 bit ADC for my application. My requirement is to read temperature from 0 deg centigrade to 60 deg centigrade with a accuracy 0.005 degrees and 1% tolerance . As it is 16 bit ADC, and I want to…
Part Number: ADS114S06B Hi ,
1. i was working with ADS114S06B and it is interfaced to Raspberry pi using spi interface. i was to unable to read any data from ADS114S06B , i was in confusion that whether the device is working or not. can you please suggest…
Part Number: ADS114S06B We are using mentioned device in one of our projects. It is interfaced with SC20. I request for the schematic review. Schematic is attached.
Control_Board.pdf
Part Number: ADS114S06B Other Parts Discussed in Thread: ADS114S06 , ADS114S08B Dear Sir/Madam,
We have built a custom board using ADS114S06BIPBS to read PT1000 sensors. But we are having issues with SPI communication. The signal line from the MCU to ADS114S06…
Part Number: ADS114S06B Other Parts Discussed in Thread: ADS114S06 Hi expert,
1. Please help review schematic of ADS114S06B.
2. Could I directly use this schematic for ADS114S06?
6735.schematic.pdf
Regards and thanks.
Jiandong
Part Number: ADS114S06B Hello,
I've seen where a ferrite bead is put in line with the power shared with digital power supplies to feed analog components. Where can I learn more about this practice and some of the tradeoffs and tuning practices? In…
Part Number: ADS114S06B We are using the ADS114S06B in our system. We have chosen this chip for it's 16 bit capabilities. This would project out input range (+-32.768V) exactly as 1mV/bit.
To keep our power supplies simple, we took the input voltage…