Part Number: ADS114S06B Hello E2E,
I am using the ADS114S06B to support two separate sensors at a time. I will have to ping-pong between the two sensors during operation. This will entail switching IDAC connections (and current value), external reference…
Part Number: ADS114S06B Other Parts Discussed in Thread: ADS114S08B Dear All,
I am using ADS114S06B as can be seen in the SCH in attachment. It was designed to measure thermocouples.
When operating my final product with power contactors, the A/D is subjected…
Part Number: ADS114S06B I want to detect over range if the analog input goes about Internal reference voltage 2.5V?
Is there any register or indication for this? If no then how detect the over range?
Part Number: ADS114S06B Hello,
I am actually doing user calibration using SYOCAL by setting the null voltage and SYGCAL by applying a Full scale i.e. 10V.
ADC is calibrating properly, but the issue is after power reset ADC showing previous values i.e…
Part Number: ADS114S06B Hi, I'm using this ADC to convert two kind of signals, 0-60mVcc / 0-10Vcc, please see attached schematic.
I need to measure 0-60mV on AIN0 channel and 0-10Vcc on AIN2 channel.
Problem found: When I apply a signal higher then…
Part Number: ADS114S06B Other Parts Discussed in Thread: AFE4400
Hello Team,
I am developing a medical device where we have two separate ground for Analog & digital via Ferrite bead.
I want to get clarity on using the separate Ground for Analog or…
Part Number: ADS114S06B Hello support team,
I have a question regarding offset and gain calibration of ADS114S06B.
Which commands and in which order must be perfirm to calibrate ADS114S06B?
Best regards,
W. Fink
Part Number: ADS114S06B Hello,
setup:
- 5V to 3.3V logic level shifter as depicted in "bidirectional converter" - https://jeelabs.org/book/1504d/
- Arduino UNO
- Arduino IDE 182
- TQFP to100 mil adapter PCB
- No 47 Ohm resistors; the rest identical…
Part Number: ADS114S06B Other Parts Discussed in Thread: ADS114S06 Hello,
I am not sure I understand the proper way to take single ended input measurements. Here is how I have tried:
byte addr, data, aux;
addr = CMD_WREG | REF_R; …
Part Number: ADS114S06 Hello,
I'm looking for further information about the current sources (IDACs). On datashhet's page 8, you say 100ppm/ºC for temperature drift (each IDAC).
This is the typical, minimum or maximun value? I do some tests…