Part Number: ADS1158 Tool/software: We are using ADS1158 with Bipolar configuration & Analog inputs are connected in differential mode. We found our design is Woking after the 1st prototype testing.
We made couple of boards using the same design and…
Part Number: ADS1158
Tool/software:
Hi,
I am unable to read the Data in the ADC channel in the Fixed Channel mode, data is incorrect.
I am applying 0.5V to the Input channel for Channel o, the value is not corresponding to the 0.5V.
Kindly…
Part Number: ADS117L18 Other Parts Discussed in Thread: ADS1158 , ADS127L18 , Tool/software: Hi all,
I am looking for a replacement for ADS1158.
[Requirements] conversion method: ΔΣ Resolution: 16bit or more Number of channels: 10ch or more (if possible…
Part Number: ADS1158 What is the height tolerance of ADS1158? The maximum is listed, but I need more information on the minimum total height which is listed at 0.90 Max.
Mechanical. Dimension. Height. Tolerance.
Part Number: ADS1158 Tool/software: Hi,
Sorry for the basic question, but I would like to know about the following question from a customer.
"Is the full-scale range when used in single-ended half that when used differentially?"
Looking at Table…
Part Number: ADS1158 Hi!
I want to check if I can use the ads1158 for this:
Reading of 16 potentiometers(analog inputs) and 8 switches(gpio) all at once directly to ADC and Spi to MCU. (0-5v)
If this is possible. What are the basic connections…
Part Number: ADS1158 Other Parts Discussed in Thread: ADS1258 Running into persistency issues with the ADS1158, specifically regarding the SPI capabilities. MOSI and MISO do not consistently provide a reliable transmission.
Part Number: ADS1158 Dear TI forum,
I have 3 x ADS1158 on a shared SPI bus. Let's call them ADC A, B and C. I am using 2 GPIOs for toggling a MUX in order to properly set the chip select pins for each ADC. The MUX is SNx4HC139. Each DRDY pins are connected…
Part Number: ADS1158 Hello! I'm using the ADS1158 for measuring some analog values, however I see that frequently the measurements will be completely wrong. I have seen this issue on 3 boards now and I believe I traced the issue down to the fact that…
Part Number: ADS1158 Other Parts Discussed in Thread: ADS1278 In Auto scan mode in ADS1158, if we are utilizing all 16 channel, and lets say I am using 8usec time delay, no chopping, and 4 averages, with this config, let's say I am getting around 800…