Part Number: ADS1174 ADS is giving only 0.2V interrupt pulses when MCU is not fetching data due to which probably MCU stop Reading Interrupt suddenly.
Moreover we are for settings we are using 2.5 VRef+ and gnd as VRef- with 25MHz crystal oscillator. and…
Part Number: ADS1174 Other Parts Discussed in Thread: ADS1274 Hi,
I am looking to design a device which requires having ADS1174 converters daisy-chained, synchronized samples, over two PCBs using a cable to connect them together (one ADC on each PCB)…
Part Number: ADS1174 Other Parts Discussed in Thread: ADS1178 Hello.
I am looking to develop a device in which the analog measurements are synchronized on UTC. The goal is to have several devices with analog measurements that are synchronized at +/- 100ns…
Part Number: ADS1174 Other Parts Discussed in Thread: THS4524 Hello, I am carrying out current measurements using Rogowski coils, one Operational amplifier THS4524, and one ADC ADS1174. When installed, the device is working 24/7 without interruption. Few…
Part Number: TUSB4041I-Q1 Other Parts Discussed in Thread: ADS1174 , , TUSB8041-Q1 Hi Team,
The package information are not complete in the datasheet, customer need the full package information like ADS1174 datasheet page 36-39. Which is using the same…
Other Parts Discussed in Thread: ADS1174 Hi All,
Presently, we are using ADS1174 to read data for 3 inputs (~2.6 V). To be simple, we are ignore DRDY pin and just clock four channel data out continuously. But unfortunately data don't look right.
…
Other Parts Discussed in Thread: ADS1174 Hi
I have a microcontroler that is clocked at 120Mhz (60MIPS internal) with a crystal oscillator where the resulting SPI interface clock is SCLK=10MHz. The ADS1174 datasheet states that CLK and SCLK must have a…
Other Parts Discussed in Thread: ADS1174 Can you comment on the ADS1174 ground plane?
The part has a thermal pad underneath which the datasheet tells me to connect to a ground plane but there is no indication as to which ground plane (analog or digital…