Part Number: ADS1198 Other Parts Discussed in Thread: ADS1194 ,
I am working on ADS1194 with Vref=2.4V
CONFIG2 = 0x30
CHnSET = 0x65
Based on datasheet with this config I should expect a 1mV calibration signal to be generated and sampled by ADS. Gain is…
Part Number: ADS1198 I am able to record data using My ADS1198 based circuit.
I have ADS1198PDK as well.
The data i am receiving is noisy in nature, they are not clean. (See the attached Image).
Even the * channel that i am receiving is noisy.
Only Lead…
Part Number: ADS1198 Other Parts Discussed in Thread: TMS320VC5507 In my project i am going to use ADS1198 and the data will be live streamed. So for that if i use the ADS1198 for its potential i.e., data rate at 8Ksps for each channel simultaneously…
Part Number: ADS1198 I am using ADS1198.
I have tested my Circuit with WCT. It is working ok except some noise.
I have ADS1198 Evaluation board as well.
Now i need to test with RLD.
Question 1: So, what sort of changes i need to do in my hardware as…
Part Number: ADS1198 I have ADS1198, i need to test pace detection.
What are the changes that i need to do in order to detect the pace.
what addition hardware is required and where will i get it ?
Part Number: ADS1198 hi,
The RLDOUT pin of the ADS1198 host does not output 1.5V when the lead is off, but outputs 3V. The waveform is as follows. This abnormality will show that the signal cannot be detected, and it always prompts that the lead is off…
Part Number: ADS1198
Hello,
How can i calculate WCT using the Lead 1, Lead 2 or even using Lead 3 ?
As
Channel 2 is Lead 1
Channel 3 is Lead 2
and Lead 3 can be calculated as
Lead 3 = Lead 2 - Lead 1.
and i need WCT
which is given by WCT = (LA+RA…
Part Number: ADS1198 Other Parts Discussed in Thread: ADS1298 Our customer plans to open a new product of ECG monitoring, which needs an 8-channel low-power ECG scheme. We plan to use ads1298 to design and be compatible with ads1198 at the same time.…
Part Number: ADS1198 Other Parts Discussed in Thread: ADS1298 , ADS1292
Hi everybody.
I'm looking for an advice about ads1188, i.e. if is it good enough for a EMG (electromyography) and it could be a good backup of a 1298.?!