Part Number: ADS1203 Dear TI Representative,
I am designing a circuit to output a 5V-0V square wave using the following circuit.
However, the output from the photocoupler remains at 0V.
What measures can I take to enable the output?
Thank you for…
Part Number: ADS1203 The ADS1203IPWT is in our application used in such a way that the negative input pin is tied to ground and mode pins are configured for mode 2, i.e. manchester encoded output using the internal oscillator.
According to the datasheet…
Part Number: AMC1303M2520 Other Parts Discussed in Thread: ADS1203 Hi team,
Does TI have any other smaller package options similar to AMC1303M2520? The customer has looked for such product information before, but couldn't find it so far. Non-isolated…
Dear Hendrick,
Thanks for reply.
We would use ADS1203 not AMC1203. I typed mistakenly AMC1203 instead of ADS1203. Isolation between cold and hot side will be done
through pulse transformer like you have given Application Note. Please suggest some…
Part Number: AMC1210MB-EVM Other Parts Discussed in Thread: ADS1204 , ADS1203 , ADS1202 , AMC1210 , , ADS1209EVM My team is using an F28379D launchpad for motor controller for a PMSM. We need to read data from the resolver to achieve this. I’m trying…
Hi Raja,
We've talked about the AMC1210 already. You mentioned as well that you were using the TMS320F280049RSH controller, which also supports Manchester decoding. The ADS1203 has an internal modulator clock, so you don't need to use a second isolation…
Part Number: TMS320F280045 Other Parts Discussed in Thread: ADS1203 Hi experts,
My customer use SINCFAST filter, OSR=128, Sdfm1Regs.SDDPARM2.bit.SH=1. When input of AMC1306 is -250mV~250mV, hey found the data fluctuates greatly. They thought that for…
Part Number: TMS320F28388D Other Parts Discussed in Thread: TIDM-02009 , ADS1203 , ADS1209 Hi team,
I’m looking for TMS320F28388D reference design for SDFM, and recommended Delta sigma modulator device to connect.
The reference designs (such like…
Holger,
Potenza SDFM example code is not yet available. Our software team is working on it. Meanwhile you can use F28377D example code in control suite for reference.
Regarding the SD modulators, it really depends upon your application. If you just…