Part Number: ADS1204 Tool/software: The ADS1204 voltage sampling circuit used was damaged, and two ADS1204 pieces were damaged on one board. The PCB photo is shown in Figure 1.
The parts in Figure 1 are divided into:
1: Damaged ADS1204, the preliminary…
Part Number: ADS1204 Other Parts Discussed in Thread: ADS1202 Tool/software: Good morning, I am looking for a representation of the ADS1204 sigma delta converter (block diagramm Z transform). In order to be able to make precision calculations of my analog…
Part Number: ADS1204 Hi,
my customer has a question regarding the impedance formula show below.
I just would like to have a confirmation: Is fMOD the CLKIN frequency or the CLKOUT frequency (fCLKIN / 2)? I guess it is the CLKOUT one but I am not sure…
Part Number: ADS1204 Team,
do we have a Matlab Simulink model of the ADS1204?
My customer seems to have one, but they are not sure if it has been modified by them or not, so they would like to get the original one.
BR
Part Number: ADS1204 Other Parts Discussed in Thread: OPA336 Hi,
We are using the ADS1204 to acquire single-sided signals on the positive side inputs. Can we connect REFOUT directly to REFIN and all negative side inputs (CH A-, CH B-, CH C-, CH D…
Part Number: ADS1204 Other Parts Discussed in Thread: AMC1204 Team,
we only specify the typical value in the datasheet. Do you have any information about the max value?
Best regards
Part Number: ADS1204 Other Parts Discussed in Thread: ADS1208 Hi team,
My customer used the ADS1204, and saw some LSB cross-talk. When a voltage is converted on channel 1, this is also visible on the other channels in a weakened form.
1. Is crosstalk…
Part Number: ADS1204 Other Parts Discussed in Thread: ADS1274 , ADS1278 Dear all,
I am searching for a delta-Sigma ADC which Outputs the bit stream directly; we want to do the Signal processing in an FPGA. I remember the ads1204 from years ago. Are…
Part Number: ADS1204 Hi,
How would the power consumption of the ADS1204 increase if we moved from using a 20 MHz external clock (10 MHz sample rate) to a 32 MHz external clock (16 MHz sample rate)? How would this increased power consumption affect…