Part Number: ADS1216 is there more information on this device?
my set up is as follows:
1.- 1st frame: 590047h = unipolar
2.- 2nd frame: 50000Ch = fosc/256, Vref int, Vre 2.5V, Buff off, MSB 1st
3.- 3thd frame: 510008h = channel 0, with COMM
4.- wait…
Part Number: ADS1216 Other Parts Discussed in Thread: ADS124S08 Hi all,
I am using the ADS1216 to measure the bipolar voltage, using only the Ain0 pin as input, with a voltage range of ± 2.5V, set according to the specification, but the test range is…
Part Number: ADS1216 Other Parts Discussed in Thread: ADS1217 See below my settings:
REFEN = 1 (internal ref)
REF HI = 1 (2.5V)
BUFEN = 0 (disable, need maximum input voltage)
My gain is still as default = 000, G=1
PSEL = 0000 (channel 0 positive)
…
Part Number: ADS1216 Hi,
I would like to ask you a question about the OCR/FCR of ADS1216.
I have studied application report "SBAA099" as below.
http://www.ti.com/analog/docs/litabsmultiplefilelist.tsp?literatureNumber=sbaa099&docCategoryId=1&familyId…
Part Number: ADS1210 Hi,
Let me post as below about reset timing of ADS1210 the other day.
https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/p/627987/2315621#2315621
After that, I also have studied other similar devices, ADS1212…
Part Number: ISO7742 Other Parts Discussed in Thread: ADS1216 , Hi
My customer has met a problem when taking a 6000V ESD Test in a RTD application by using ADS1216 and ISO7742.
MCU will make a self-test for the register, and if there's something wrong in…
Other Parts Discussed in Thread: ADS1216 , ADS1217 , ADS1218 Hi,
I wonder if anyone could communicate an arduino Uno with an ADS1216. In case I need the code if someone has this project. Thank you
Part Number: ADS1216 Other Parts Discussed in Thread: ADS124S08 , ADS124S06 it is 2.47V after power on,then slowly reduced to 2.41V.Is there a possibility that I have bought a fake one?
Other Parts Discussed in Thread: ADS1216 Hi all,
We have the ADS1216 component.
We have a problem, when connecting a battery to our analog input, we read the first 12 bits stable. But the 12 less significant bits are changing all the time. I'm trying to…