Part Number: ADS1220 Other Parts Discussed in Thread: ADS124S08 Hi Sir,
Our customer want to find a solution to replace AD4130-4. We suggest ADS1220 but our current spent higher than ADI device. Is there any suggestion to compete with AD4130-4? Thanks…
Part Number: ADS1220 Hello
I am configuring the ADC according to the following to read the input voltage provided at AIN0:
Config Reg 0: 0x81
Config Reg 1: 0x04
Config Reg 2: 0xD8
Config Reg 3: 0x00
I am using the ADC in unipolar mode: AVDD:5V; AVSS…
Part Number: ADS1220 Hi team,
In my customer application, the use the ads1220 with internal clock and the sps is been set as 1000 sps but for many ads1220 devices. Some will be 980 sps and the others may be 1020 sps , the clock pin connected to gnd by…
Hi Étienne,
This isn't specifically spelled out as computation time as several things are going on. In the section I referenced before (8.5.1.3) regarding DRDY it mentions where the pulse goes high for 2*tmod (note modulator periods and not tclk…
Part Number: ADS1220 Dear Expert
Due to the inconsistency between the configuration frequency and output data rate of the ADC chip ADS1220IPW in the pressure detection board, the board cannot be used normally. Exception description: The DR bit of software…
Part Number: ADS1220 Other Parts Discussed in Thread: MSPM0L1106 , , ADS1248 , ADS1148 , ADS1260 , ADS124S06 , MSPM0L1306 , TPSM365R15 The application is to measure wire resistance from 0 to 2200 ohms with a sub-milliohm resolution in order to calculate the…
Part Number: ADS1220 Dears,
Customer Feedback that when they use ADS1220 ,end customer feedback below questions:
1. Now the ADS1220 is connected with a K-type thermocouple, and the temperature collected by the feedback from the end customer is very unstable…
Part Number: ADS1220 Hi,
I have customer who are having problems testing with the ADS1220.
The customer normally tests the ADS1220 current of about 10-12uA, but recently using the same test board to test another batch of chips found that the current reached…
Part Number: ADS1220 Hello : )
I was wondering if you can help me. I currently plan on having several SPI devices on the same bus - and some of these devices including the ADS1220 can have their supplies powered down. I'd like the devices on the bus that…
Part Number: ADS1220 Dear Experts,
i currently have strange Problems with the ADS1220 that i can not wrap my head around.
We're essentially using the reference Layout to measure a thermocoupler connected to AIN0 and AIN1.
While fixing bugs in our…