Part Number: ADS1220 Hello Team,
in the datasheet it is recommended for the Rf resistors not to be higher than 1K.
If I can accept:
reduction of the dynamic due to the input current flowing through the Rf
increased differential error due to Rf misma…
Part Number: ADS1220 Other Parts Discussed in Thread: OPA2197 , Hi TI Technical Support Team,
I am planning to use TI ADS1220 24 bit ADC in single ended mode. I will measure two inputs, one will vary between 0.5V and 4.5V and the other input will vary between…
Part Number: ADS1220 We are using ADS1220 in one of our RTD applications and the datasheet mentions that the current match is +/-0.3%.
Does this value increase with the loading?
Part Number: ADS1220 capicitor C422 report.xlsx
Hello
using the ADS1220 to get the load cell data but facing the issue of voltage variation as voltage is mV (measurement range 0.800mV-10mV)
Using the configuration in my design as well as in ads1220…
Part Number: ADS1220 Hi,
The ads1220 maximum sampling rate is 2ksps. Is it the same when using one channel and all four channels?
Is it 500sps per channel when using 4 channels?
Regards,
Part Number: ADS1220
I am facing noise problems with ADS1220.
I got placed ADS1220 ADC and a GSM module on the same multi-layer board. When GSM starts transmitting, measurements of ADS1220 starts being inflated.
For reducing amount of problems I am now…
Part Number: ADS1220 Hi,
We have been using the ADS1220 for a wheatstone bridge sensor and now we would like to do temperature measurements using the int ernal temp erature sensor as well. However, we found that data received from the ADS1220 is mixed up…
Part Number: ADS1220
Hi Experts,
Good day.
Cx is using multiple ADS1220 A/D converters for a design. Was going to share the DRDY pin between all ADS1220s they're using. They'll have isolated CS input lines for each A/D, but was wondering if sharing the…
Part Number: ADS1220 Hi, I have problem with SPI data rate on ADS1220.
I've been setup turbo mode and 2000 sps.
It seems ADS1220 just responded 60-80 sps. (Sometimes the DRDY pin is inactive too long, so I must send reset command and init again).
I don…