Other Parts Discussed in Thread: ADS1222 , MSP430F5436A , MSP430F5436 , ADS1224 , REF5025 Hi,
Currently I design a data logger board which need 4 channel analog input. I use 4 ADS1222 and one MSP430F5436A. Now I have some questions need clarify. Please help…
Other Parts Discussed in Thread: ADS1222 One of the features listed for the ADS1222 is a +/- 5V differential input range. However, maximum rating indicates that the analog input voltage to gnd can only go from -0.3 to VCC + 0.3. Moreover, the voltage…
Other Parts Discussed in Thread: ADS1222 I've read the datasheet of ADS1222, but I didn't find the decimatior of it.
The output would be 120Hz with 2MHz operating frequency.
I wonder whether it do the resampling and choose the average?
Tks! …
Part Number: ADS1248 Other Parts Discussed in Thread: ADS1251 , ADS1225 , ADS1222 , ADS1224 , ADS1226 Hi,
I would like to ask you a simple question about the calibration.
The data sheet of ADS1248 describes about calibration as below. (40page)
According…
Other Parts Discussed in Thread: ADS1222 , REF5025 , REF5050 , OPA2335 Hi there,
I'm designing a circuit which uses an ADS1222 to perform 16-bit ADC conversions out of an inclinometer (SCA103T for what matters).
The circuitry includes two reference voltage…
Sorry for using the forum as a social platform...
We use the SCA103T inclinometer a lot, and so far most of our projects used only the SPI communication - and I can say, with quite excellent results.
I am right now working on an analog interface, and…
Other Parts Discussed in Thread: ADS1220 , ADS1220EVM Hi,
I am testing the ADS1220 for type B thermocouple measurement for a commercial product. I purchased the EV1220 unit, but I found it easier to use the Arduino Mega for the testing. Eventually, in production…
Hello,
thanks for your fast reply.
We do reset and adjusting for offset only one time at startup.
Anyway it is a pairing issue as you suspected.
We have an HSP051-4N10 to protect differential signals against
EDS between channels. Without it the issue…