Part Number: ADS122C04 Tool/software: Dear Specialists,
My customer is interested in ADS122C04 and has a question about current consumption at power up.
I would be grateful if you could advise.
---
According to the datasheet, there are various…
Part Number: ADS122C04 Other Parts Discussed in Thread: ADS1015 , ADS112C04 Tool/software: Hi,
I am using this chip, could anyone tell me what the driver is in the latest Linux kernel 6.10.2. Thank you!
Part Number: ADS122C04 Tool/software: I have worked with this device on 4 different applications, device works well.
The problem is that my newest application hangs up occasionally when I write to a register or acquire data. There is one main difference…
Part Number: ADS122C04 Tool/software: Hi, I'm Junhyeob from the Korea.
I have been using ADS122C04 as a single device on the board.
Now, I have to design a multiple ADS122C04 test board.
On the datasheet, ADS122C04 can have different 16 I2C addresses…
Part Number: ADS122C04 hi, Dear product line engineer.
my customer has inquire: whether or not is there any register for store chip ID and revision in ADS122C04? my understanding is no. Am I right? thanks.
regards,
Bill
Part Number: ADS122C04 1. Under the condition of single power supply, can the differential input mode be negative (i.e. Vp<Vn)? 2. If the internal reference voltage 2.048V is used, how should the REFP and REFN pins be connected? Should they refer to this…
Part Number: ADS122C04 We are using Ain0 and Ain1 to measure a pseudo-differential ±2.0V signal. We have ±2.5V for AVDD and AVSS and are using AVDD and AVSS as references. The current termination of the signal before the ADC inputs is a configuration…
Part Number: ADS122C04 Hello,
We're considering to use ADS122C04 for reading floating voltage source sensors like pyranometer. I've been experimenting with the circuit and tried to set the input common mode voltage by connecting the negative input to…
Part Number: ADS122C04 Hello,
I try to get my head around this but I cannot find an issue.
I see depending on the gain different amount of deviations:
Following is the wiring diagram. To the ADC a strain bridge simulator is connected, simulating…
Part Number: ADS122C04 I am seeing a reading on one channel being affected by the voltage on another channel. Confirmed the actual voltages on the pins are as expected.
The problem can be solved by reading the channel twice and only using the second…