Part Number: ADS1230 I have a question regarding to ADS1230. Question is following:
What logic level appears on DRDY/DOUT pin, when PDWN pin is set to L?
I would expect Hi-z, but diagram o datasheet page 19 shows Hi!
Thanks
Ludek Pavlus
Part Number: ADS1230 I am having a load-cell connected with ADS1230. ADS1230 is interfaced with 8bit STM8s controller. while operating system on 5V, ADS1230 is giving 0xFFFFF value, i'm not getting the conversion as per loadcell voltage changes. While…
Part Number: ADS1230 HI
I want to work with ads1230 with my processor(stm32f103)
SCLK pin Clocks are fine , 20 clocks for data conversion and 4 additional clocks to force the Dout pin goes Hi
i saw the Dout pin and sclk pin on oscope , they are fine…
Part Number: ADS1232 Other Parts Discussed in Thread: ADS1230 Tool/software: Hello,
My company has been using the ADS-1232 since 2010, with an annual production of around 2,000 boards for load cell reading. We have never encountered any issues until…
Part Number: ADS1230 Hello Sir,
we are using ads1230 in our current project.
GAIN: 128
SPEED: 10SPS
REFP: 2.5V
REFN: GND
code of ads1230 interface is on bit banging.
ADS1230 normal works ok. but some time give spike like 0x3FFF , 0x7FFF etc. reading.
…
Part Number: ADS1230 Hi, Could you tell me aboute ADS1230 conversion time accuracy? I want to know the sampling time accuracy when operating at 80 SPS. ex) 80SPS→12.5ms ± xx% Best Regards, Yusuke
Part Number: ADS1230 Hi everyone, I'm not sure to well understand what does the offset calibration on the ADS1230.
I see two solutions:
1) the ADS1230 creates an internal short to have an input voltage of 0mv and take a measurement. The result should…
Part Number: ADS1231 Other Parts Discussed in Thread: ADS1230 , ADS1232 , ADS1220 Hi,
How to change the gain of the internal amplifier present in the ADS1231.