Part Number: ADS1231 Hi,
I have downloaded and installed an analog engineers calculator. I can't able to select device parameters kindly help me to set it up
Thanks & Regards
navin
Part Number: ADS1231 Hi Bob,
I have made the corrections that you suggested. Now more fluctuations are happening. Kindly, Help me to get the non fluctuated results.
Thanks & Regards
Navin Chakravarthy
Part Number: ADS1231
Hello! I'm trying to get some outputs, but I think I don't understand the values.
I'm trying to give a 0 V input so the ADS can give me the value of 000000h. The schematic is the following:
Where AINP-AINN = 0 mV, so…
Part Number: ADS1231 HI,
I have faced the issues to convert Adcvalue to the weight which is from ads1231. Kindly help me to work on this
Thanks & Regards
Navin Chakravarthy K
Part Number: ADS1231 Hi,
I already use the ADS1231 in a previous board and it worked well.
Now I just reviewed this board and I noted that the measure was very noisy.
I configured the ADC with speed high. At the power on I send a power down pulse at PDWn…
Hi Navin,
The conversion from voltage to weight is dependent on the sensitivity of the load cell. Load cell sensitivity is given by the manufacturer as mV/V which refers to the output of the load cell per voltage of excitation to achieve the full scale…
Part Number: ADS1231
Hi team,
I would like to know about ADS1231,what is its maximum weight it can measure? this is the sample loadcell I am having www.vetek.com/.../article
Best regards,
Part Number: ADS1231 Hello There!, I'm using the ADS1231 with the reference schematic. I have tried to read data, but nothing happens. I have checked the DOUT signal when I set PDWN to high and SCLK to low, and it makes 100ms period pulses. The thing…
Part Number: ADS1231 Other Parts Discussed in Thread: MSP430F5529 Hello,
I am facing some problems regarding the output codes of the ADS1231. According to Table 3 in the ADS1231's datasheet, I should be receiving a code of 0x00 when there is no weight…
Part Number: ADS1231 Other Parts Discussed in Thread: MSP430F5529 , Hello,
I'm using the following code to communicate between an ADS1231 and MSP430F5529 in my weight scale design. The resulting data is shown below. As you can see, the last two bytes…