Hi Akash,
It is not clear what you are saying is the issue and you haven't given us any data as an example. What are your expectations? What is your input voltage?
The SELFCAL of the ADS1241 will remove device offset and gain error. It is important…
Part Number: ADS1241 Other Parts Discussed in Thread: ADS124S08 Hi !
I want to measure a temperature with a voltage divider and a NTC thermistor. The range of the measure is 0-5V and I use a voltage reference chip (5V to supply the ADS, the voltage…
Part Number: ADS1241 I am working on ADS1241. I have applied 37.1 mV differentially. My code is working fine in polling mode but when I took it to interrupt it malfunctioned. For some time it gives 37.1 mV but after that it comes to 9.6 mV.
Please find…
Part Number: ADS1241 I am using an ADS1241 to measure a thermocouple. It works fine at PGA gain=1 or PGA gain=2. But it starts giving numbers as PGA gain is increased. I have tried the Self Gain Calibration (SELFGCAL) command but it doesn't seem to do…
Other Parts Discussed in Thread: ADS1241 , TL431 , STRIKE Hi,
We're facing new problem: ADS1241 stops responding completely (for commands read/write registers and reading data).
We're using ADS1241 in different units in the past without problems.…
Helge,
Do you know if this customer question has been answered?
I wanted to include something to this post so that other readers could benefit from this thread. I've already sent this to you, but there is an older application note on using crystal…
Other Parts Discussed in Thread: ADS1241 , LM4128 I am using the ADS1241 to measure thermocouples (J-type).
I have a Fluke Thermocouple Calibrator that one can set the temperature to a value and it will generate the voltage that a thermocouple would…
Other Parts Discussed in Thread: ADS1241 Hi, I am using the ADS1241 to read two thermcouples.
I am having some timing issues. What I am doing is setting the mux to amplify between channels 4 and 5, then reading the output value, then I am changing the…