Other Parts Discussed in Thread: ADS1241 Hi, I am using the ADS1241 to read two thermcouples.
I am having some timing issues. What I am doing is setting the mux to amplify between channels 4 and 5, then reading the output value, then I am changing the…
Other Parts Discussed in Thread: ADS1241 , REF5025 I am using an ADS1241 ADC to read some thermocouple in a noisy environment. Since the ADS1241 is directly connected to the outside world, I am using a ADUM3154 to isolate the SPI signals from the microcontroller…
Other Parts Discussed in Thread: ADS1241 Hello, all
Now we have some inquiries regarding /DRDY on ADS1241 from our customer.
Please refer to the items below, and feedback us with your comment.
1) Rising on /DRDY
When referring to the datasheet of this device…
Hi Bob,
I am working with two ADS1241 and would like to switch between the two and read the data when DRDY pin on each chip goes low. Having these two separate interrupts, I have tried turning the other chip off before writing to the mux register and reading…
Other Parts Discussed in Thread: ADS1241 , ADS1220 I am having trouble understanding the external voltage reference and its relation to the ACR's RANGE bit on the ADS1241. I want to sample a voltage source that ranges from 0 to 5V.
I power the chip…
Other Parts Discussed in Thread: ADS1241 I read the posts on the ads1241 and while some of that made sense I'm still a little in the dark concerning the proper sequencing of commands to minimize settling time error.
Oscillator frequency is 4.9152 …
Other Parts Discussed in Thread: ADS1241 Hello there,
actually I'm dealing with the ADS1241 24Bit ADC. For a first quick evaluation, I want to use that device together with the MMB0 EVM Motherboard and the ADC-PRO Ver. 2 software. The MMB0 is designed…
Other Parts Discussed in Thread: ADS1241 Using the ads1241 on a number of boards with a number of different power configurations. On one of these boards the ads1241 sometimes comes up in a mode where it is does not digitize the signal correctly and results…
Other Parts Discussed in Thread: ADS1241 Hello,
I am trying to use the ADS1241, but I can't find anywhere that states specifically what the data transfer rate is. I see that the individual channel sampling rate is 15Hz (I am using a 4.9152MHz crystal…