Part Number: ADS1246 I have a problem when using ads1246. There are 8 ads1246 on my circuit board, and the MCU(STM32) is used to control these 8 ads1246.
1. Use just one pin of the MCU to control 8 ads1246's START,
2.Use 8 pins of the MCU to monitor…
Part Number: ADS1246 Other Parts Discussed in Thread: OPA333 , TIPD120 Hi Team,
My customer would like to use ADS1246 pspice model to run simulation, for the purpose of getting more accuracy result my customer would like to know whether the model build…
Part Number: REF5025 Other Parts Discussed in Thread: ADS1246
Hi,
I'm using a REF5025 connected to a ADS1246
I have a very strange behavior: at start-up, the ref output does not reach the target 2.5V. It stays below 1V. Sometimes, after a random…
Part Number: ADS1246 Hi,
For testing basic functionality of the ADS1246 I created a basic setup (see attached schematic). For reading out the data I'm using an ESP32. I can successfully read and write the command registers of ADS1246. But the /DRDY PIn…
Part Number: ADS1246 Dear TI expert
When debugging ADS1246, appear to ADS1246 register write is not successful, but read the sampling data of the normal phenomenon, MUC and ADS1246 is not a piece of circuit boards, SPI by 30 cm + FPC1.0 rows of connection…
Part Number: ADS1246 Other Parts Discussed in Thread: ADS1230 , ADS1232 , ADS1231 , ADS1220 , ADS1235 , ADS124S06 Hi Everyone,
I am planning to use the AD1246 with a load cell at 3.3V operation.
1. Can is still use the the 2.048V reference or is it better…
Part Number: ADS1246 Other Parts Discussed in Thread: ADS1247 , ADS1248 Hello, I recently purchased a few ADS1246 to accurately measure the voltage on a laser diode thermistor. I am using an Arduino Uno to interface with the chip and am using a power supply…
Part Number: ADS1246
Hello,
This thread is in the continuity of :
https://e2e.ti.com/support/data-converters/f/73/t/741611
and
https://e2e.ti.com/support/data-converters/f/73/t/753350
Even after we changed our Vref voltage from 3V to 1.8V, we are still…
Part Number: ADS1246 Hi TI engineers,
My digital interface resources is limited, I have only 4 isolated SPI interface between ADS1246 and CPU, As is described in the datasheet, PIN 14 can function as both DOUT and DRDY, So leave PIN13 DRDY floating…