Part Number: ADS1248 Tool/software: Hello Team,
Could you please share Radiation Report for ADS1248? I couldn't find it on TI.com or in data sheet.
Thank you in advance.
Part Number: ADS1248 Tool/software: Hi friends, I have interface Stm32f103c8t6 microcontroller with ADS1248 ADC to find the temperature value using PT1000 sensor. I got all necessary files for circuit design and source code for ADS1248 ADC in TI…
Part Number: ADS1248 Tool/software: Hi,
I have designed a 4-channel, 2-wire PT1000 sensor interface using the ADS1248 IC and written the firmware based on the datasheet for my design. I successfully obtained the ADC output for all 4 channels, which…
Part Number: ADS1248 Tool/software: We are using ADS1248 for 3-Wire RTD(PT-100) sensor measurement. but there is sudden drop in Temperature as i attached picture, so i tested it.. Could you help me if this waveforms are phenomenon that could reasonable…
Part Number: ADS1248 Other Parts Discussed in Thread: ADS124S08 Tool/software: At present, we use ADS1248 for pressure sampling, and the ADC sampling value begins to increase abnormally. When the ambient temperature exceeds 100 ℃, the applied ambient…
Part Number: ADS1248 Other Parts Discussed in Thread: ADS124S08 Tool/software: Hi,
We are using ADS1248, 24-bit ADC chip to interface with STM32 controller via SPI Communication. We have not got proper output ADC value. When always read the ADC value get…
Part Number: ADS1248 Other Parts Discussed in Thread: STRIKE , , ADS124S08 Dear Bryan,
With reference to our previous discussions on this topic, I appreciate if you could clarify some information from the device datasheet:
The specified device input…
Hi Chuck Wong,
Chuck Wong said: As we both can see, both ±2.5V voltages were impacted when the U1 and U8 goes bad. Do you have any insights as on why the ADS1248 is holding down their supplies to a bad level?
If the ADCs are holding down the supplies,…
Part Number: ADS1248 What's up TI,
We have used ADS1248 for many years with 1000 ohm 2 mV/V strain gauges, 2 mA constant current (1 mA x 2 in parallel) and 3.6VDC rails. Internal reference, 1 ksps. We have tens of thousands in the field with very…