Hi Mojie,
Mojtaba Aghaalian said: The datasheet says preferably set that voltage to 1/2 AVDD. Why 1/2? Because it is in the middle of comparator dynamic range?
Setting at AVDD/2 allows for the proper common-mode for the PGA input over all PGA gain settings…
Hi Nimish,
Nimish Palod said: We are configuring register 0x04 setting its value to 0x17 for 100SPS with Low Latency filter in both the cases (1.47 gain and unity gain). We tried configuring some more registers but there was no difference found. Also…
Part Number: ADS124S08 Hi, I am using ADS124S08 for my project. It has a 24bit resolution but I am getting values equivalent to 23bit resolution. The max reading I am getting is 8388607, while according to 24 bit resolution it should be around 16777215…
Hi Emre ARSANACI,
Since your original question has been resolved, I moved your new question to a new post: https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1308441/ads124s08-issues-with-reading-data-from-ads124s0…
Other Parts Discussed in Thread: ADS124S08 Hi Bryan,
I solve this but I got new problem.
When I change the INMUX from AIN0 and AIN1 to AIN2 to AIN3, I got nothing.
Here is my steps;
I set the configuratıon like internal voltage, gain and INMUX AIN2 to…
Part Number: ADS124S08
Dear Technical Support Team,
I'd like to measure 2cases range of temperature with 3-Wire RTD for PT100.
①0℃~150℃ ⇒ 100Ω~157.33Ω
②0~400℃ ⇒ 100~247.09Ω(Expand from ① 157.33Ω to 247.09Ω)…
Part Number: ADS124S08 Hello, TI
I have an ADS124S08 that I'm working to implement into a larger project. I have a few things I want to measure with it, but for now, I'm playing with measuring an RTD. I'm getting what I think are good readings, but the…
Part Number: ADS124S08 Other Parts Discussed in Thread: ISOW7741 , ADS1261 , , ADS1220 , ADS1263 Hello,
I have to measure temperature using RTDs installed within the coils of a 460V AC variable frequency motor.
The current off-the-shelf DAQ module is quite…
Hi Bob
Bob Benjamin said: Also, when using the GUI the LP should not be connected. When the LP is used JP1 installed will place the EVM in a reset state and shuts down the communication capability of the onboard processor.
we followed the same step.
we…