Part Number: ADS124S08 Hello, TI
I have an ADS124S08 that I'm working to implement into a larger project. I have a few things I want to measure with it, but for now, I'm playing with measuring an RTD. I'm getting what I think are good readings, but the…
Part Number: ADS124S08 Other Parts Discussed in Thread: ISOW7741 , ADS1261 , , ADS1220 , ADS1263 Hello,
I have to measure temperature using RTDs installed within the coils of a 460V AC variable frequency motor.
The current off-the-shelf DAQ module is quite…
Hi Bob
Bob Benjamin said: Also, when using the GUI the LP should not be connected. When the LP is used JP1 installed will place the EVM in a reset state and shuts down the communication capability of the onboard processor.
we followed the same step.
we…
Part Number: ADS124S08 Hello team,
Is the sampling rate of ADC limited to less than 60SPS, when using 50-Hz and 60-Hz Line Cycle Rejection?
On the datasheet, it says "The digital filter provides enhanced rejection of power-line-coupled noise for data rates…
Part Number: ADS124S08 Other Parts Discussed in Thread: ADS125H02 , ADS1261 , , ADS1262 Hi.
I want to develop a data acquisition device (DAQ).
The quantities I want to measure are as follows:
1) RTD (2/3/4 wires)
2)Thermocouples
3) 0-20ma/4-20ma current…
Part Number: ADS124S08 Hello, TI
I have been attempting to learn how to use the ADS124S08 for a larger project. The method of communication I want to use is relatively simple: the Microprocessor sends a command over the SPI interface to read data, the…
Part Number: ADS124S08 Hello,
I have a thermopile sensor that gives min-max output between -1.4 mV and 180 mV. I used the ADS124S08 integration and gave the output of the thermopile directly to the ADC integration. This is the schematic drawing of the…
Part Number: ADS124S08 Other Parts Discussed in Thread: ADS125H02 Hello Team, We are planning to use the ADC ADS124S08 for one of our applications to measure the temperature using RTD sensors like (PT100 and PT1000). The excitation current of 1mA for the…
Part Number: ADS124S08 Hi team,
When using ads124s08 to sample a large resistance, it takes 300ms to get the accurate value. The values sampled at 40ms and 100ms have a large deviation separately. Now customer suspected that the low-pass filter they were…
Part Number: ADS124S08 Hi,
I have interface ADS124S08 With STM32F746 Controller. I have facing issued with register reading. I have checked on the CRO and Found that Whatever data i have sending its properly show on the MOSI Line but MISO Pin did not…