Part Number: ADS1252 Other Parts Discussed in Thread: ADS127L11 , ADS1260 For the ADS1252U the Documentation Of the equivalent circuit shows two separate clock pins onboard. In the Doc it discusses running the CLK as a 16Mhz speed, can this be done using…
Part Number: ADS1252 Other Parts Discussed in Thread: ADS1256 , ADS1255 Hi,
Is it possible to provide IBIS model of digital interface on ADS1252?
Thanks and best regards, M.HATTORI.
Part Number: ADS1252 We are planning to use ADS1252 for our new product. We would like to know whether this is an end-of life product. We expect it to be used for at least 5 years
Regards
Kumaravel.G
Part Number: ADS1252 Other Parts Discussed in Thread: ADS127L11
Hi,
Just want to confirm, the ADS1252 do not have adjustable sample rate, correct?
Do we have other alternative with a adjustable sampling rate with a this parameters below - 24 bits…
Part Number: ADS1252 Hi
My Customer has question.
The customer confirmed the operation as shown below using ADS1252. Confirmed when CLK was stopped and restarted with input voltage applied. Is this phenomenon normal for ADS1252?
ADS1252.pdf
Best…
Part Number: ADS1252 Other Parts Discussed in Thread: TLC3541 Hi,
Could you please let us know the input capacitor of CLK (Device System Clock) pin on ADS1252U?
Thanks and best regards, M.HATTORI.
Part Number: ADS1252 For the convenience of the system, we are thinking of acquiring data in 1tDRDY cycle. (Of course, 5 cycles after start-up are discarded.) We hope the evidence that there is no problem even if only the 6th cycle data is applied as…
Part Number: ADS1252 Other Parts Discussed in Thread: ISO224 , OPA2350 Hello,
I have one problem. I would like to measure voltage form +5V to -5V, with 41667Hz rate, with my ADS1252 chip.
Are there is a certain circuit for my application on web…
Part Number: ADS1252 Hi
Read the value from ADS1252, the values change in rules. The CLK is 9M.
Please help check the following code:
u32 ADS1252_Red(void) { u32 recevice=0,i=0; while(ADS1252_Out==1); while(ADS1252_Out==0); while(ADS1252_Out==1…
Part Number: ADS1252 Other Parts Discussed in Thread: ADS1220 , ADS124S06 , REF6025 Hi sir,
I have ADS1252 ADC .
I want to interface K-type, THERMOCOUPLE with ADS1252 directly.!
Is there any application Note ,sample Code for this Measurement Available…