Part Number: ADS1256EVM-PDK Hello,
I hope you are well,
Customer is having problem with part:
ADS1256EVM-PDK
DC: 2335
LOT: 3013717SVT
PO: 029-6N843
Invoice date to Customer: 2023-10-27
Claim made by Customer:
ADS1256EVM-PDK customer…
Part Number: ADS1256EVM-PDK Hi Team,
My customer is using ADS1256EVM, and is having trouble with the setup.
After connect the EVM to MMB0, DRDY output normally as below.
However, after removing the MMB0 and trying to send commands below through…
Part Number: ADS1256EVM-PDK Other Parts Discussed in Thread: ADS1256 , Hello
I am integrating the ADS1256 to my project
can i have the altium file of the ADS1256EVM-PDK to get the symbols and librairies from
best regards
Ziad JABBOUR
Part Number: ADS1256EVM-PDK Other Parts Discussed in Thread: ADCPRO , ADS1256 Hello.
I'm having a problem to read data from my ADS1256EVM directly.
I can retrieve data from it using ADCPro software if I use PDK together.
It means my ADS1256EVM…
Part Number: ADS1256EVM-PDK Other Parts Discussed in Thread: ADS1256 Hello
I was trying to get some layout help for the ADS1256. The Gerber files that I downloaded from the EVM-PDK page on your website has most of the layers blank. Only GBS and GTS…
Part Number: ADS1256EVM-PDK Other Parts Discussed in Thread: ADCPRO , ADS1256 Hi, Good day. Our customer is using the ADS1256EVM-PDK and they have the following observations and question. "I've purchased an ADS1256evm-pdk for evaluation of the mentioned…
Part Number: ADS1256EVM-PDK Other Parts Discussed in Thread: ADCPRO , ADS1256 I am using ADS1256EVM with Raspberry Pi 3 with source code High-Precision-AD-DA-Board-Code.7z
I have tried with wires connection in readme.txt of source code and set up switches…
Hi Mehul,
Did you download and install the "ADS1256EVM-PDK-SW" from this page: www.ti.com/.../ads1256evm-pdk
If you still have issues aftter this installation, please try running the MMB0 driver installer located at "C:\Program Files (x86)\ADCPro…
Part Number: ADS1256EVM-PDK Hi Team,
I understand that the DRDY is goes low if the ADC data is available for retrieval. A customer wants to confirm if the ADC data corrupted if DRDY goes high during the channel readout.
Regards,
Danilo