Part Number: ADS125H01 I have a number of these A/D's (ADS125H01) that I want to keep in sync with each other. They are run off a common clock (7.3728MHz) and they have all their start pins tied together. I was intending to start all the converter…
Part Number: ADS125H01 Hello-
I have been working with my ADS125H01 design (schematic attached) and I noticed that if I power down the HV_AVDD (+12V) and AVDD (+5V) rails, my register settings are lost and need to be re-set. I couldn't find anything in…
Part Number: ADS125H01 Other Parts Discussed in Thread: ADS125H02 , ADS125H02EVM Dear Specialists,
My customer is interested in ADS125H01 and wants to obtain EVM.
But I couldn't find it.
Could you please let us know when is ADS125H01EVM released.
I…
Part Number: ADS125H01ADS125H01 Main Status (STATUS0) Register (address = 01h) [reset = 01h],shows that there is a Reference Voltage Alarm (bit three of this register),This bit sets when the reference voltage falls below < 0.4 V (typical). The alarm…
Part Number: ADS125H01 Other Parts Discussed in Thread: ADS125H02 , Hi There-
I've been working with the ADS125H01 and its sister part ADS125H02 in a load cell application. I have 12V, 5V, and 3.3V available on my board, and the load cell is excited at…
Part Number: ADS125H01ADS125H01 cannot read and write registers whose addresses exceed 10H, even if CS2(low active) has been pulled down.
Figure 1 below is the write register function (WREG Command), and Figure 2 is the SPI read-write array for single…
Part Number: ADS125H01 Hello,
I would like to make clear the input range,
I use +/-15V supply and do not ground my system and the measured one, only the differential input + is connected to 18V and the diferential input - is connected to -1V. It means…
Part Number: ADS125H01 Please recommend a 24 bit ΣΔ ADC With Rail-to-Rail OPAMP ADC. In addition, it requires small volume, low price and no requirement for sampling rate.
Part Number: ADS125H01 Other Parts Discussed in Thread: ADS1260 Hi team,
My customer would like to design one solution that can measure uA current measurement solution.
The specification is measuring 0~50mA current and the current shunt resistor will be…
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS1260 , ADS125H01 , ADS1235 , ADS1261 The customer is looking for a ADC for Bridge type pressure sensor. 24Bit and 10k SPS.
Whether ADS131M02 could be used in this application?
If not, why?
I also…