Part Number: ADS1260 Other Parts Discussed in Thread: ADS125H02
We are using ADS1260 and ADS125H02 in our design,
For sensor exictation we are using Internal reference from the ADC.
Is it ok to put out the reference output of the ADC to the connector…
Part Number: ADS1260 Other Parts Discussed in Thread: TPS7A20 , TPS61099 , REF6025 , TPS784 , TPS63700 , TPS7A30
Hi Team,
Thank you for suggestion.
After discussion of ADS1260’s ability, it could meet/approach our requirement.
Now I have some questions…
Part Number: ADS1260 Hi, I want to measure a signal between 0V - 2V5 with the ADS1260. For this I use the internal reference (REF(06h) = 10h). The PGA is set in bypass mode (PGA(10h) = 80h). The multiplexer is set to AIN0 and AINCOM (INPMUX(11h) = 10h). AVDD…
Part Number: ADS1260 Other Parts Discussed in Thread: ADS1261EVM Hi sir,
For the uA solution of ADS1260:
-R-shunt = 500mΩ for much buffer of avoiding noise.
-Vref = 4.5V
-Vshunt_Max = Isense_Max x Rshunt = 50mA x 500mΩ = 25mV
-Dynamic Range…
Part Number: ADS1260 Other Parts Discussed in Thread: REF6045 , REF6025 Hi bro,
For the uA solution of ADS1260:
If I choose bigger value R-shunt = 500mΩ for much buffer of avoiding noise,
(1) Vshunt_Max = Isense_Max x Rshunt = 50mA x 500mΩ = 25…
Part Number: ADS1261EVM Other Parts Discussed in Thread: ADS1260 , , ADS1235 , ADS125H01 , ADS1261 , REF6025 Hello,
I would like to design a solution that can measure uA current measurement solution.
Here's the specification:
1. Measure 0~50mA current.
2. We…
Part Number: ADS1260 Hi Team,
I have a question about ADS1260 PGA offset voltage. ADS1260 PGA Vos is ±50/gain uV_typ. Is this input referred offset voltage?
which calculation is correct? calculation A gain=10 Vout={(INA-INB)±50uV}*gain
Calculation…
Part Number: ADS1260 Currently, I would like to acquire digital data obtained by converting analog inputs from AIN0 to AIN3 with ADS1260 in order (at the same time as possible). I have a question about the procedure and speed at that time. About the pr…
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS1260 , ADS125H01 , ADS1235 , ADS1261 The customer is looking for a ADC for Bridge type pressure sensor. 24Bit and 10k SPS.
Whether ADS131M02 could be used in this application?
If not, why?
I also…
Hi Team,
My customer would like to know the accuracy and temperature drift in the 10uA range.
I found that the URN-OUT CURRENT SOURCES accuracy at 0.05uA is in the datasheet.
But it's not in the 10uA range.
Please let us know the specifications. …